TI BLE5-Stack API Documentation  2.02.07.00
Data Fields
hciEvt_BLEExtCteConnectionIqReport_t Struct Reference

LE Extended CTE Connection IQ Report Event. More...

Data Fields

uint8 BLEEventCode
 BLE Event Code.
 
uint16 connEvent
 connection event
 
uint16 connHandle
 connection handle
 
uint8 cteType
 cte type
 
uint8 dataChIndex
 index of data channel
 
uint8 dataLen
 samples data length
 
uint8 eventIndex
 event number
 
osal_event_hdr_t hdr
 osal event header
 
void * iqSamples
 list of interleaved I/Q samples (list size is dataLen*2)
 
uint8 phy
 current phy
 
uint16 rssi
 current rssi
 
uint8 rssiAntenna
 antenna ID
 
uint8 sampleCtrl
 sample control - default filtering or RAW_RF
 
uint8 sampleRate
 sample rate (1/2/3/4 MHz)
 
uint8 sampleSize
 sample size (8 or 16 bit)
 
uint8 slotDuration
 sampling slot 1us or 2us
 
uint8 status
 packet status (success or CRC error)
 
uint16 totalDataLen
 samples data length includes in all next events
 

Detailed Description

LE Extended CTE Connection IQ Report Event.


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale