TI BLE5-Stack API Documentation  2.02.07.00
Data Fields
gapSlaveSecurityReqEvent_t Struct Reference

Data Fields

uint8_t authReq
 
uint16_t connectionHandle
 Connection Handle.
 
uint8_t deviceAddr [B_ADDR_LEN]
 address of device requesting security
 
osal_event_hdr_t hdr
 GAP_MSG_EVENT and status
 
uint8_t opcode
 GAP_SLAVE_REQUESTED_SECURITY_EVENT
 

Detailed Description

GAP_SLAVE_REQUESTED_SECURITY_EVENT message format.

This message is sent to the app when a Slave Security Request is received.

This event will be consumed by the gapbondmgr if it exists.

Field Documentation

§ authReq

uint8_t authReq

Authentication Requirements

Bit 2: MITM, Bits 0-1: bonding (0 - no bonding, 1 - bonding)


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale