TI BLE5-Stack API Documentation  2.02.07.00
Data Fields
gapDeviceInitDoneEvent_t Struct Reference

Data Fields

uint16_t dataPktLen
 HC_LE_Data_Packet_Length.
 
uint8_t devAddr [B_ADDR_LEN]
 Device's public or random static address.
 
osal_event_hdr_t hdr
 GAP_MSG_EVENT and status
 
uint8_t numDataPkts
 HC_Total_Num_LE_Data_Packets.
 
uint8_t opcode
 GAP_DEVICE_INIT_DONE_EVENT
 

Detailed Description

GAP_DEVICE_INIT_DONE_EVENT message format.

This message is sent to the app when the Device Initialization is done [initiated by calling GAP_DeviceInit ].


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale