TI BLE5-Stack API Documentation  2.02.07.00
Data Fields
deviceTypeRspPld_t Struct Reference

Data Fields

uint8_t chipFamily
 Chip Family Field from ChipInfo module.
 
uint8_t chipType
 Chip Type Field from ChipInfo module.
 
uint8_t cmdID
 Ext Ctrl Op-code.
 
uint8_t hardwareRev
 Hardware revision Field from ChipInfo module.
 
uint8_t rsvd
 RFU.
 

Detailed Description

Response to a OAD_EXT_CTRL_GET_DEV_TYPE command

For information on how to interpret the fields below, see the ChipInfo module within the device's driverlib documentation


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale