TI BLE5-Stack API Documentation  2.02.07.00
Data Fields
attFlowCtrlViolatedEvt_t Struct Reference

ATT Flow Control Violated Event message format. More...

Data Fields

uint8 opcode
 opcode of message that caused flow control violation
 
uint8 pendingOpcode
 opcode of pending message
 

Detailed Description

ATT Flow Control Violated Event message format.

The following two ATT events are generated locally (not received OTA) by the ATT Server or Client. This message is sent as a GATT_MSG_EVENT of method ATT_FLOW_CTRL_VIOLATED_EVENT to the app by the local ATT Server or Client when a sequential ATT Request-Response or Indication-Confirmation protocol flow control is violated for a connection. All subsequent ATT Requests and Indications received by the local ATT Server and Client respectively will be dropped.

This message is to inform the app (that has registered with GAP by calling GAP_RegisterForMsgs) in case it wants to drop the connection.


The documentation for this struct was generated from the following file:
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale