TI BLE5-Stack API Documentation
2.02.07.00
|
Modules | |
Micro BLE Stack Callbacks | |
Micro BLE Stack Constants | |
Micro BLE Stack Structures | |
Files | |
file | uble.h |
This file contains configuration, initialization, and parameter management of Micro BLE Stack. It also contains interfacing between Micro BLE Stack and the application. | |
Macros | |
#define | BLE_LOG_INT_INT(handle, type, format, param1, param2) |
#define | BLE_LOG_INT_STR(handle, type, format, param1, param2) |
#define | BLE_LOG_INT_TIME(handle, type, start_str, param1) |
Functions | |
bStatus_t | uble_checkAddr (ubleAddrType_t addrType, uint8 *pAddr) |
Check if the given address is valid. More... | |
bStatus_t | uble_getAddr (ubleAddrType_t addrType, uint8 *pAddr) |
Retrieve the address corresponding to the given address type. More... | |
bStatus_t | uble_getParameter (uint8 param, void *pValue) |
Get a Micro BLE Stack parameter. More... | |
void | uble_processMsg (void) |
Let the Micro Stack process the queued messages. More... | |
bStatus_t | uble_registerAntSwitchCB (ubleAntSwitchCB_t pfnAntSwitchCB) |
Register callback for antenna switch. More... | |
void | uble_resetAddr (void) |
Make BD Addr revert to Random Static Address if exists or Public Address otherwise. | |
bStatus_t | uble_setParameter (uint8 param, uint8 len, void *pValue) |
Set a Micro BLE Stack parameter. More... | |
bStatus_t | uble_stackInit (ubleAddrType_t addrType, uint8 *pStaticAddr, ublePostEvtProxyCB_t pfnPostEvtProxyCB, uint8 timeCritical) |
Initialize Micro BLE Stack. More... | |
uint8 | uble_timeCompare (uint32 time1, uint32 time2) |
This function determines if the first time parameter is greater than the second time parameter, taking timer counter wrap into account. If so, TRUE is returned. More... | |
uint32 | uble_timeDelta (uint32 time1, uint32 time2) |
This function determines the difference between two time parameters, taking timer counter wrap into account. More... | |
bStatus_t uble_checkAddr | ( | ubleAddrType_t | addrType, |
uint8 * | pAddr | ||
) |
Check if the given address is valid.
addrType | - UBLE_ADDRTYPE_PUBLIC , UBLE_ADDRTYPE_STATIC , UBLE_ADDRTYPE_NONRESOLVABLE , or UBLE_ADDRTYPE_RESOLVABLE |
pAddr | - pointer to where the address to check resides |
bStatus_t uble_getAddr | ( | ubleAddrType_t | addrType, |
uint8 * | pAddr | ||
) |
Retrieve the address corresponding to the given address type.
addrType | - UBLE_ADDRTYPE_PUBLIC , UBLE_ADDRTYPE_STATIC or UBLE_ADDRTYPE_BD |
pAddr | pointer to memory location to return address. This should be a uint8_t[6] |
bStatus_t uble_getParameter | ( | uint8 | param, |
void * | pValue | ||
) |
Get a Micro BLE Stack parameter.
param | - parameter ID: Micro BLE Stack Parameters |
pValue | - pointer to location to get the value. This is dependent on the parameter ID and WILL be cast to the appropriate data type (example: data type of uint16 will be cast to uint16 pointer). |
void uble_processMsg | ( | void | ) |
Let the Micro Stack process the queued messages.
bStatus_t uble_registerAntSwitchCB | ( | ubleAntSwitchCB_t | pfnAntSwitchCB | ) |
Register callback for antenna switch.
pfnAntSwitchCB | - application antenna switch callback |
bStatus_t uble_setParameter | ( | uint8 | param, |
uint8 | len, | ||
void * | pValue | ||
) |
Set a Micro BLE Stack parameter.
param | - parameter ID: Micro BLE Stack Parameters |
len | - length of data to write |
pValue | - pointer to data to write. This is dependent on the parameter ID and WILL be cast to the appropriate data type (example: data type of uint16 will be cast to uint16 pointer). |
bStatus_t uble_stackInit | ( | ubleAddrType_t | addrType, |
uint8 * | pStaticAddr, | ||
ublePostEvtProxyCB_t | pfnPostEvtProxyCB, | ||
uint8 | timeCritical | ||
) |
Initialize Micro BLE Stack.
addrType | - Micro BLE Stack Address Types Type of the address which the device will use initially. Either UBLE_ADDRTYPE_PUBLIC or UBLE_ADDRTYPE_STATIC . If addrType is UBLE_ADDRTYPE_PUBLIC , the public address which is stored in CCFG preferably or in FCFG otherwise will be used for BD Addr. If addrType is UBLE_ADDRTYPE_STATIC , BD Addr will depend on pBDAddr. |
pStaticAddr | - If this is NULL and addrType is UBLE_ADDRTYPE_STATIC , a random static address will be generated by the stack and will be used for BD Address. If this is not NULL and addrType is UBLE_ADDRTYPE_STATIC , the 6 byte-long data pointed to by pBDAddr will be used for BD Address as the random static address. |
pfnPostEvtProxyCB | - Callback to trigger a context switch to the application task so that the messages queued by the stack can be processed by uble_processMsg in the application task context. |
timeCritical | - rf transmit operation. For strict timing on the transmission, set value to RF_TIME_CRITICAL. For relaxed timing on the transmission set value to RF_TIME_RELAXED. |
uint8 uble_timeCompare | ( | uint32 | time1, |
uint32 | time2 | ||
) |
This function determines if the first time parameter is greater than the second time parameter, taking timer counter wrap into account. If so, TRUE is returned.
time1 | - First time. |
time2 | - Second time. |
uint32 uble_timeDelta | ( | uint32 | time1, |
uint32 | time2 | ||
) |
This function determines the difference between two time parameters, taking timer counter wrap into account.
time1 | - First time. |
time2 | - Second time. |