TI BLE5-Stack API Documentation  2.02.07.00
Macros

Macros

#define ATT_ERR_ATTR_NOT_FOUND   0x0a
 No attribute found within the given attribute handle range.
 
#define ATT_ERR_ATTR_NOT_LONG   0x0b
 Attribute cannot be read or written using the Read Blob Request or Prepare Write Request.
 
#define ATT_ERR_INSUFFICIENT_AUTHEN   0x05
 The attribute requires authentication before it can be read or written.
 
#define ATT_ERR_INSUFFICIENT_AUTHOR   0x08
 The attribute requires an authorization before it can be read or written.
 
#define ATT_ERR_INSUFFICIENT_ENCRYPT   0x0f
 The attribute requires encryption before it can be read or written.
 
#define ATT_ERR_INSUFFICIENT_KEY_SIZE   0x0c
 The Encryption Key Size used for encrypting this link is insufficient.
 
#define ATT_ERR_INSUFFICIENT_RESOURCES   0x11
 Insufficient Resources to complete the request.
 
#define ATT_ERR_INVALID_HANDLE   0x01
 Attribute handle value given was not valid on this attribute server.
 
#define ATT_ERR_INVALID_OFFSET   0x07
 Offset specified was past the end of the attribute.
 
#define ATT_ERR_INVALID_PDU   0x04
 The attribute PDU was invalid.
 
#define ATT_ERR_INVALID_VALUE   0x80
 The attribute value is invalid for the operation.
 
#define ATT_ERR_INVALID_VALUE_SIZE   0x0d
 The attribute value length is invalid for the operation.
 
#define ATT_ERR_PREPARE_QUEUE_FULL   0x09
 Too many prepare writes have been queued.
 
#define ATT_ERR_READ_NOT_PERMITTED   0x02
 Attribute cannot be read.
 
#define ATT_ERR_UNLIKELY   0x0e
 The attribute request that was requested has encountered an error that was very unlikely, and therefore could not be completed as requested.
 
#define ATT_ERR_UNSUPPORTED_GRP_TYPE   0x10
 The attribute type is not a supported grouping attribute as defined by a higher layer specification.
 
#define ATT_ERR_UNSUPPORTED_REQ   0x06
 Attribute server doesn't support the request received from the attribute client.
 
#define ATT_ERR_WRITE_NOT_PERMITTED   0x03
 Attribute cannot be written.
 

Detailed Description

© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale