TI-15.4 Stack API  5.30.00.26
Data Fields
_apimac_securitypibkeyusageentry Struct Reference

#include <api_mac.h>

Data Fields

uint16_t keyIndex
 
uint8_t keyUsageIndex
 
ApiMac_keyUsageDescriptor_t usageEntry
 

Detailed Description

Security PIB Key ID usage entry for a Get/Set ApiMac_securityAttribute_keyUsageEntry

Field Documentation

§ keyIndex

uint16_t _apimac_securitypibkeyusageentry::keyIndex

index into the macKeyUsageList

§ keyUsageIndex

uint8_t _apimac_securitypibkeyusageentry::keyUsageIndex

index into macKeyUsageList[keyIndex]

§ usageEntry

ApiMac_keyUsageDescriptor_t _apimac_securitypibkeyusageentry::usageEntry

Place to put the requested data


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale