TI-15.4 Stack API  5.30.00.26
Data Fields
_apimac_securityleveldescriptor Struct Reference

#include <api_mac.h>

Data Fields

uint8_t frameType
 
uint8_t commandFrameIdentifier
 
uint8_t securityMinimum
 
bool securityOverrideSecurityMinimum
 

Detailed Description

Security Level Descriptor

Field Documentation

§ frameType

uint8_t _apimac_securityleveldescriptor::frameType

Frame Type

§ commandFrameIdentifier

uint8_t _apimac_securityleveldescriptor::commandFrameIdentifier

Command Frame ID

§ securityMinimum

uint8_t _apimac_securityleveldescriptor::securityMinimum

The minimal required/expected security level for incoming MAC frames.

§ securityOverrideSecurityMinimum

bool _apimac_securityleveldescriptor::securityOverrideSecurityMinimum

Indication of whether originating devices for which the Exempt flag is set may override the minimum security level indicated by the Security Minimum element. If TRUE, this indicates that for originating devices with Exempt status, the incoming security level zero is acceptable.


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale