TI-15.4 Stack API  5.30.00.26
Data Fields
_apimac_sdata Struct Reference

#include <api_mac.h>

Data Fields

uint8_t * p
 
uint16_t len
 

Detailed Description

Data buffer structure

Field Documentation

§ p

uint8_t* _apimac_sdata::p

pointer to the data buffer

§ len

uint16_t _apimac_sdata::len

length of the data buffer


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale