TI-15.4 Stack API  5.30.00.26
Data Fields
_apimac_payloadieitem Struct Reference

#include <api_mac.h>

Data Fields

bool ieTypeLong
 
uint8_t ieId
 
uint16_t ieContentLen
 
uint8_t * pIEContent
 

Detailed Description

Structure a Payload information Item

Field Documentation

§ ieTypeLong

bool _apimac_payloadieitem::ieTypeLong

True if payload IE type is long

§ ieId

uint8_t _apimac_payloadieitem::ieId

IE ID

§ ieContentLen

uint16_t _apimac_payloadieitem::ieContentLen

IE Content Length - max size 2047 bytes

§ pIEContent

uint8_t* _apimac_payloadieitem::pIEContent

Pointer to the IE's content


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale