TI-15.4 Stack API  5.30.00.26
Data Fields
_apimac_mrfskphydesc Struct Reference

#include <api_mac.h>

Data Fields

uint32_t firstChCentrFreq
 
uint16_t numChannels
 
uint32_t channelSpacing
 
uint8_t fskModScheme
 
uint16_t symbolRate
 
uint8_t fskModIndex
 
uint8_t ccaType
 

Detailed Description

Generic PHY Descriptor. We are using this structure for both Channel Page 9 and Channel Page 10.

Field Documentation

§ firstChCentrFreq

uint32_t _apimac_mrfskphydesc::firstChCentrFreq

First Channel Center frequency

§ numChannels

uint16_t _apimac_mrfskphydesc::numChannels

Number of channels defined for the particular PHY mode

§ channelSpacing

uint32_t _apimac_mrfskphydesc::channelSpacing

Distance between Adjacent center channel frequencies

§ fskModScheme

uint8_t _apimac_mrfskphydesc::fskModScheme

2-FSK/2-GFSK/4-FSK/4-GFSK

§ symbolRate

uint16_t _apimac_mrfskphydesc::symbolRate

Symbol rate selection

§ fskModIndex

uint8_t _apimac_mrfskphydesc::fskModIndex

Modulation index as a value encoded in MR-FSK Generic PHY Descriptor IE (IEEE802.15.4g section 5.2.4.20c).
2FSK MI = 0.25 + Modulation Index * 0.05
4FSK MI is a third of 2FSK MI

§ ccaType

uint8_t _apimac_mrfskphydesc::ccaType

Channel clearance algorithm selection


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale