TI-15.4 Stack API  5.30.00.26
Data Fields
_apimac_mlmepollind Struct Reference

#include <api_mac.h>

Data Fields

ApiMac_sAddr_t srcAddr
 
uint16_t srcPanId
 
bool noRsp
 

Detailed Description

MAC_MLME_POLL_IND type

Field Documentation

§ srcAddr

ApiMac_sAddr_t _apimac_mlmepollind::srcAddr

Address of the device sending the data request

§ srcPanId

uint16_t _apimac_mlmepollind::srcPanId

Pan ID of the device sending the data request

§ noRsp

bool _apimac_mlmepollind::noRsp

indication that no MAC_McpsDataReq() is required. It is set when MAC_MLME_POLL_IND is generated, to simply indicate that a received data request frame was acked with pending bit cleared.


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale