TI-15.4 Stack API  5.30.00.26
Data Fields
_apimac_mlmedisassociatereq Struct Reference

#include <api_mac.h>

Data Fields

ApiMac_sec_t sec
 
ApiMac_sAddr_t deviceAddress
 
uint16_t devicePanId
 
ApiMac_disassocateReason_t disassociateReason
 
bool txIndirect
 

Detailed Description

MLME disassociate request type

Field Documentation

§ sec

ApiMac_sec_t _apimac_mlmedisassociatereq::sec

The security parameters for this message

§ deviceAddress

ApiMac_sAddr_t _apimac_mlmedisassociatereq::deviceAddress

The address of the device with which to disassociate

§ devicePanId

uint16_t _apimac_mlmedisassociatereq::devicePanId

The PAN ID of the device

§ disassociateReason

ApiMac_disassocateReason_t _apimac_mlmedisassociatereq::disassociateReason

The disassociate reason

§ txIndirect

bool _apimac_mlmedisassociatereq::txIndirect

Transmit Indirect


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale