TI-15.4 Stack API  5.30.00.26
Data Fields
_apimac_mlmedisassociateind Struct Reference

#include <api_mac.h>

Data Fields

ApiMac_sAddrExt_t deviceAddress
 
ApiMac_disassocateReason_t disassociateReason
 
ApiMac_sec_t sec
 

Detailed Description

MAC_MLME_DISASSOCIATE_IND type

Field Documentation

§ deviceAddress

ApiMac_sAddrExt_t _apimac_mlmedisassociateind::deviceAddress

The address of the device sending the disassociate command

§ disassociateReason

ApiMac_disassocateReason_t _apimac_mlmedisassociateind::disassociateReason

The disassociate reason

§ sec

ApiMac_sec_t _apimac_mlmedisassociateind::sec

The security parameters for this message


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale