TI-15.4 Stack API  5.30.00.26
Data Fields
_apimac_mcpspurgecnf Struct Reference

#include <api_mac.h>

Data Fields

ApiMac_status_t status
 
uint8_t msduHandle
 

Detailed Description

MCPS purge confirm type

Field Documentation

§ status

ApiMac_status_t _apimac_mcpspurgecnf::status

The status of the purge request operation

§ msduHandle

uint8_t _apimac_mcpspurgecnf::msduHandle

Application-defined handle value associated with the data request


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale