TI-15.4 Stack API  5.30.00.26
Data Fields
_apimac_mcpsdatareq Struct Reference

#include <api_mac.h>

Data Fields

ApiMac_sAddr_t dstAddr
 
uint16_t dstPanId
 
ApiMac_addrType_t srcAddrMode
 
uint8_t msduHandle
 
ApiMac_txOptions_t txOptions
 
uint8_t channel
 
uint8_t power
 
uint8_t * pIEList
 
uint16_t payloadIELen
 
ApiMac_fhDispatchType_t fhProtoDispatch
 
uint32_t includeFhIEs
 
ApiMac_sData_t msdu
 
ApiMac_sec_t sec
 
uint8_t gpOffset
 
uint8_t gpDuration
 

Detailed Description

MCPS data request type

Field Documentation

§ dstAddr

ApiMac_sAddr_t _apimac_mcpsdatareq::dstAddr

The address of the destination device

§ dstPanId

uint16_t _apimac_mcpsdatareq::dstPanId

The PAN ID of the destination device

§ srcAddrMode

ApiMac_addrType_t _apimac_mcpsdatareq::srcAddrMode

The source address mode

§ msduHandle

uint8_t _apimac_mcpsdatareq::msduHandle

Application-defined handle value associated with this data request

§ txOptions

ApiMac_txOptions_t _apimac_mcpsdatareq::txOptions

TX options bit mask

§ channel

uint8_t _apimac_mcpsdatareq::channel

Transmit the data frame on this channel

§ power

uint8_t _apimac_mcpsdatareq::power

Transmit the data frame at this power level

§ pIEList

uint8_t* _apimac_mcpsdatareq::pIEList

pointer to the payload IE list, excluding termination IEs

§ payloadIELen

uint16_t _apimac_mcpsdatareq::payloadIELen

length of the payload IE

§ fhProtoDispatch

ApiMac_fhDispatchType_t _apimac_mcpsdatareq::fhProtoDispatch

Freq hopping Protocol Dispatch - RESERVED for future use, should be cleared.

§ includeFhIEs

uint32_t _apimac_mcpsdatareq::includeFhIEs

Bitmap indicates which FH IE's need to be included

§ msdu

ApiMac_sData_t _apimac_mcpsdatareq::msdu

Data buffer

§ sec

ApiMac_sec_t _apimac_mcpsdatareq::sec

Security Parameters

§ gpOffset

uint8_t _apimac_mcpsdatareq::gpOffset

Transmit Delay for Green Power

§ gpDuration

uint8_t _apimac_mcpsdatareq::gpDuration

Transmit Window for Green Power


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale