TI-15.4 Stack API  5.30.00.26
Data Fields
_apimac_macmlmeassociatereq Struct Reference

#include <api_mac.h>

Data Fields

ApiMac_sec_t sec
 
uint8_t logicalChannel
 
uint8_t channelPage
 
uint8_t phyID
 
ApiMac_sAddr_t coordAddress
 
uint16_t coordPanId
 
ApiMac_capabilityInfo_t capabilityInformation
 

Detailed Description

MLME associate request type

Field Documentation

§ sec

ApiMac_sec_t _apimac_macmlmeassociatereq::sec

The security parameters for this message

§ logicalChannel

uint8_t _apimac_macmlmeassociatereq::logicalChannel

The channel on which to attempt association

§ channelPage

uint8_t _apimac_macmlmeassociatereq::channelPage

The channel page on which to attempt association

§ phyID

uint8_t _apimac_macmlmeassociatereq::phyID

Identifier for the PHY descriptor

§ coordAddress

ApiMac_sAddr_t _apimac_macmlmeassociatereq::coordAddress

Address of the coordinator with which to associate

§ coordPanId

uint16_t _apimac_macmlmeassociatereq::coordPanId

The identifier of the PAN with which to associate

§ capabilityInformation

ApiMac_capabilityInfo_t _apimac_macmlmeassociatereq::capabilityInformation

The operational capabilities of this device


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale