TI-15.4 Stack API  5.30.00.26
Data Fields
_apimac_keydevicedescriptor Struct Reference

#include <api_mac.h>

Data Fields

uint16_t deviceDescriptorHandle
 
bool uniqueDevice
 
bool blackListed
 

Detailed Description

Key Device Descriptor

Field Documentation

§ deviceDescriptorHandle

uint16_t _apimac_keydevicedescriptor::deviceDescriptorHandle

Handle to the DeviceDescriptor

§ uniqueDevice

bool _apimac_keydevicedescriptor::uniqueDevice

True if the device is unique

§ blackListed

bool _apimac_keydevicedescriptor::blackListed

This key exhausted the frame counter.


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale