TI-15.4 Stack API  5.30.00.26
Data Fields
_apimac_keydescriptor Struct Reference

#include <api_mac.h>

Data Fields

ApiMac_keyIdLookupDescriptor_tkeyIdLookupList
 
uint8_t keyIdLookupEntries
 
ApiMac_keyDeviceDescriptor_tkeyDeviceList
 
uint16_t keyDeviceListEntries
 
ApiMac_keyUsageDescriptor_tkeyUsageList
 
uint8_t keyUsageListEntries
 
uint8_t key [APIMAC_KEY_MAX_LEN]
 
uint32_t frameCounter
 

Detailed Description

Key Descriptor

Field Documentation

§ keyIdLookupList

ApiMac_keyIdLookupDescriptor_t* _apimac_keydescriptor::keyIdLookupList

A list identifying this KeyDescriptor

§ keyIdLookupEntries

uint8_t _apimac_keydescriptor::keyIdLookupEntries

The number of entries in KeyIdLookupList

§ keyDeviceList

ApiMac_keyDeviceDescriptor_t* _apimac_keydescriptor::keyDeviceList

A list indicating which devices are currently using this key, including their blacklist status.

§ keyDeviceListEntries

uint16_t _apimac_keydescriptor::keyDeviceListEntries

The number of entries in KeyDeviceList

§ keyUsageList

ApiMac_keyUsageDescriptor_t* _apimac_keydescriptor::keyUsageList

A list indicating which frame types this key may be used with.

§ keyUsageListEntries

uint8_t _apimac_keydescriptor::keyUsageListEntries

The number of entries in KeyUsageList

§ key

uint8_t _apimac_keydescriptor::key[APIMAC_KEY_MAX_LEN]

The actual value of the key

§ frameCounter

uint32_t _apimac_keydescriptor::frameCounter

PIB frame counter in 802.15.4 is universal across key, but it makes more sense to associate a frame counter with a key.


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale