TI-15.4 Stack API  5.30.00.26
Data Fields
_apimac_coexist Struct Reference

#include <api_mac.h>

Data Fields

uint8_t beaconOrder
 
uint8_t superFrameOrder
 
uint8_t finalCapSlot
 
uint8_t eBeaconOrder
 
uint8_t offsetTimeSlot
 
uint8_t capBackOff
 
uint16_t eBeaconOrderNBPAN
 

Detailed Description

Coexistence Information element content type

Field Documentation

§ beaconOrder

uint8_t _apimac_coexist::beaconOrder

Beacon Order field shall specify the transmission interval of the beacon

§ superFrameOrder

uint8_t _apimac_coexist::superFrameOrder

Superframe Order field shall specify the length of time during which the superframe is active (i.e., receiver enabled), including the Beacon frametransmission time

§ finalCapSlot

uint8_t _apimac_coexist::finalCapSlot

Final CAP slot

§ eBeaconOrder

uint8_t _apimac_coexist::eBeaconOrder

Enhanced Beacon Order field specifies the transmission interval of the Enhanced Beacon frames in a beacon enabled network

§ offsetTimeSlot

uint8_t _apimac_coexist::offsetTimeSlot

Time offset between periodic beacon and the Enhanced Beacon.

§ capBackOff

uint8_t _apimac_coexist::capBackOff

Actual slot position in which the Enhanced Beacon frame is transmitted due to the backoff procedure in the CAP

§ eBeaconOrderNBPAN

uint16_t _apimac_coexist::eBeaconOrderNBPAN

NBPAN Enhanced Beacon Order field specifies the transmission interval between consecutive Enhanced Beacon frames in the nonbeacon-enabled mode


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale