TI-15.4 Stack API  5.30.00.26
Data Fields
_apimac_capabilityinfo Struct Reference

#include <api_mac.h>

Data Fields

bool panCoord
 
bool ffd
 
bool mainsPower
 
bool rxOnWhenIdle
 
bool security
 
bool allocAddr
 

Detailed Description

Structure defines the Capabilities Information bit field.

Field Documentation

§ panCoord

bool _apimac_capabilityinfo::panCoord

True if the device is a PAN Coordinator

§ ffd

bool _apimac_capabilityinfo::ffd

True if the device is a full function device (FFD)

§ mainsPower

bool _apimac_capabilityinfo::mainsPower

True if the device is mains powered

§ rxOnWhenIdle

bool _apimac_capabilityinfo::rxOnWhenIdle

True if the device's RX is on when the device is idle

§ security

bool _apimac_capabilityinfo::security

True if the device is capable of sending and receiving secured frames

§ allocAddr

bool _apimac_capabilityinfo::allocAddr

True if allocation of a short address in the associate procedure is needed.


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale