SRAM_MMR

Instance: SRAM_MMR
Component: SRAM_MMR
Base address: 0x58035000


General Purpose RAM

TOP:SRAM_MMR Register Summary

Register Name

Type

Register Width (Bits)

Register Reset

Address Offset

Physical Address

PER_CTL

RW

32

0x0000 0000

0x0000 0000

0x5803 5000

PER_CHK

RW

32

0x0000 0000

0x0000 0004

0x5803 5004

PER_DBG

RW

32

0x0000 0000

0x0000 0008

0x5803 5008

MEM_CTL

RW

32

0x0000 0000

0x0000 000C

0x5803 500C

MEM_STA

RW

32

0x0000 0000

0x0000 0010

0x5803 5010

TOP:SRAM_MMR Register Descriptions

TOP:SRAM_MMR:PER_CTL

Address Offset 0x0000 0000
Physical Address 0x5803 5000 Instance 0x5803 5000
Description Parity Error Control
Parity error check controls
Type RW
Bits Field Name Description Type Reset
31:9 RESERVED9 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000
8 PER_DISABLE Parity Status Disable

0: A parity error will update PER_CHK.PER_ADDR field
1: Parity error does not update PER_CHK.PER_ADDR field
RW 0
7:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. 0b000 0000
0 PER_DEBUG_ENABLE Parity Error Debug Enable

0: Normal operation
1: An address offset can be written to PER_DBG.PER_DEBUG_ADDR and parity errors will be generated on reads from within this offset
RW 0

TOP:SRAM_MMR:PER_CHK

Address Offset 0x0000 0004
Physical Address 0x5803 5004 Instance 0x5803 5004
Description Parity Error Check
Parity error check results
Type RW
Bits Field Name Description Type Reset
31:24 RESERVED24 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x00
23:0 PER_ADDR Parity Error Address Offset
Returns the last address offset which resulted in a parity error during an SRAM read. The address offset returned is always the word-aligned address that contains the location with the parity error. For parity faults on non word-aligned accesses, CPU_SCS:BFAR.ADDRESS will hold the address of the location that resulted in parity error.
RO 0x00 0000

TOP:SRAM_MMR:PER_DBG

Address Offset 0x0000 0008
Physical Address 0x5803 5008 Instance 0x5803 5008
Description Parity Error Debug
Parity error check debug address setting
Type RW
Bits Field Name Description Type Reset
31:24 RESERVED24 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x00
23:0 PER_DEBUG_ADDR Debug Parity Error Address Offset
When PER_CTL.PER_DEBUG is 1, this field is used to set a parity debug address offset. The address offset must be a word-aligned address. Writes within this address offset will force incorrect parity bits to be stored together with the data written. The following reads within this same address offset will thus result in parity errors to be generated.
RW 0x00 0000

TOP:SRAM_MMR:MEM_CTL

Address Offset 0x0000 000C
Physical Address 0x5803 500C Instance 0x5803 500C
Description Memory Control
Controls memory initialization
Type RW
Bits Field Name Description Type Reset
31:8 MEM_SEL Memory Instance Select

This field is used to enable/disable initialization of each SRAM instance when triggered using MEM_CTL.MEM_CLR_EN. Each bit corresponds to the respective SRAM instance.

bit[x]:
0: Initialization of instance x is disabled
1: Initialization of instance x is enabled
RW 0x00 0000
7:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000
1 MEM_BUSY Memory Busy status

0: Memory accepts transfers
1: Memory controller is busy during initialization. Read and write transfers are not performed.
RO 0
0 MEM_CLR_EN Memory Contents Initialization enable

Writing 1 to MEM_CLR_EN will start memory initialization. The contents of all byte locations will be initialized to 0x00. MEM_BUSY will be 1 until memory initialization has completed.
RW 0

TOP:SRAM_MMR:MEM_STA

Address Offset 0x0000 0010
Physical Address 0x5803 5010 Instance 0x5803 5010
Description Memory Status
Controls memory initialization
Type RW
Bits Field Name Description Type Reset
31:8 MEM_STA Memory Instance Status

This field gives the current status of each SRAM instance. When an instance is being initialized the corresponding bit is set to 1, 0 otherwise.

bit[x]:
0 : Instance x is in normal mode
1 : Instance x is getting initialized
RO 0x00 0000
7:0 RESERVED0 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x00