Instance: FLASH
Component: FLASH
Base address: 0x58030000
Thor1M Flash sub-system registers, includes the NoWrapper Flash Memory Controller (NW), flash read path, and an integrated Efuse controller and EFUSEROM.
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
RW |
32 |
0xFFFF FFFF |
0x0000 0000 |
0x5803 0000 |
|
RW |
32 |
0x0000 003F |
0x0000 0004 |
0x5803 0004 |
|
RO |
32 |
0x0000 0000 |
0x0000 001C |
0x5803 001C |
|
RW |
32 |
0x0000 0000 |
0x0000 0024 |
0x5803 0024 |
|
RW |
32 |
0x0000 0200 |
0x0000 002C |
0x5803 002C |
|
RW |
32 |
0x0000 0000 |
0x0000 003C |
0x5803 003C |
|
RW |
32 |
0x0000 0000 |
0x0000 0040 |
0x5803 0040 |
|
RW |
32 |
0x0000 0000 |
0x0000 0050 |
0x5803 0050 |
|
RW |
32 |
0x0000 0000 |
0x0000 0054 |
0x5803 0054 |
|
RW |
32 |
0x0000 0000 |
0x0000 0058 |
0x5803 0058 |
|
RW |
32 |
0x0000 0000 |
0x0000 005C |
0x5803 005C |
|
RW |
32 |
0x0000 0000 |
0x0000 0060 |
0x5803 0060 |
|
RW |
32 |
0x0000 0000 |
0x0000 0064 |
0x5803 0064 |
|
RW |
32 |
0x0000 0000 |
0x0000 0068 |
0x5803 0068 |
|
RW |
32 |
0x0000 0000 |
0x0000 006C |
0x5803 006C |
|
RW |
32 |
0x0055 9400 |
0x0000 0070 |
0x5803 0070 |
|
RW |
32 |
0x1920 0000 |
0x0000 0074 |
0x5803 0074 |
|
RW |
32 |
0x00B4 C53A |
0x0000 0078 |
0x5803 0078 |
|
RW |
32 |
0x0000 0000 |
0x0000 1000 |
0x5803 1000 |
|
RW |
32 |
0x0000 0000 |
0x0000 1004 |
0x5803 1004 |
|
RW |
32 |
0x0000 0000 |
0x0000 1008 |
0x5803 1008 |
|
RW |
32 |
0x0000 0000 |
0x0000 100C |
0x5803 100C |
|
RW |
32 |
0x0000 0001 |
0x0000 1010 |
0x5803 1010 |
|
RO |
32 |
0x0000 0001 |
0x0000 1014 |
0x5803 1014 |
|
RO |
32 |
0x0000 0000 |
0x0000 1018 |
0x5803 1018 |
|
RW |
32 |
0x0000 0000 |
0x0000 101C |
0x5803 101C |
|
RO |
32 |
0x0000 0000 |
0x0000 1020 |
0x5803 1020 |
|
RW |
32 |
0x0000 0000 |
0x0000 1024 |
0x5803 1024 |
|
RO |
32 |
0xXXXX XXXX |
0x0000 1028 |
0x5803 1028 |
|
RO |
32 |
0x0000 XXXX |
0x0000 102C |
0x5803 102C |
|
RW |
32 |
0x0000 0000 |
0x0000 1030 |
0x5803 1030 |
|
RW |
32 |
0x0000 0000 |
0x0000 1034 |
0x5803 1034 |
|
RW |
32 |
0x0000 0000 |
0x0000 1038 |
0x5803 1038 |
|
RW |
32 |
0x0000 0000 |
0x0000 103C |
0x5803 103C |
|
RO |
32 |
0x0000 0000 |
0x0000 1040 |
0x5803 1040 |
|
RO |
32 |
0x0000 0000 |
0x0000 1044 |
0x5803 1044 |
|
RW |
32 |
0x0000 0000 |
0x0000 1048 |
0x5803 1048 |
|
RW |
32 |
0x0000 0000 |
0x0000 104C |
0x5803 104C |
Address Offset | 0x0000 0000 | ||
Physical Address | 0x5803 0000 | Instance | 0x5803 0000 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | WEPROT_B0_31_0_BY1 | Internal. Only to be used through TI provided API. | RW | 0xFFFF FFFF |
Address Offset | 0x0000 0004 | ||
Physical Address | 0x5803 0004 | Instance | 0x5803 0004 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:6 | RESERVED6 | Internal. Only to be used through TI provided API. | RO | 0b00 0000 0000 0000 0000 0000 0000 | ||
5 | WEPROT_B1_ENGR_BY1 | Internal. Only to be used through TI provided API. | RW | 1 | ||
4 | WEPROT_B0_ENGR_BY1 | Internal. Only to be used through TI provided API. | RW | 1 | ||
3 | WEPROT_B1_TRIM_BY1 | Internal. Only to be used through TI provided API. | RW | 1 | ||
2 | WEPROT_B0_TRIM_BY1 | Internal. Only to be used through TI provided API. | RW | 1 | ||
1 | WEPROT_B1_FCFG_BY1 | Internal. Only to be used through TI provided API. | RW | 1 | ||
0 | WEPROT_B0_CCFG_BY1 | Internal. Only to be used through TI provided API. | RW | 1 |
Address Offset | 0x0000 001C | ||
Physical Address | 0x5803 001C | Instance | 0x5803 001C |
Description | NW and Efuse Status | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:17 | RESERVED15 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 | ||
16 | STALLSTAT | An ocp1 or ocp3 read stall has occurred. 0 : No stall or stall acknowledged by writing a 1 1 : Stall condition occurred/occurring This is a read/write-clear status bit. It will reset to 0. It will be set when either an ocp1 or ocp3 read occurs to a bank that is presently undergoing a program or write operation. An ocp2 write of 1 to this bit will clear the bit. The ocp2 write will take highest priority in the event an ocp1/ocp3 read is occurring concurrently to the ocp2 write. Clearing the bit should be done only after the ongoing program/erase operation is complete indicating that both banks are free. If clearing occurs while the stall condition persists, the field may get set back to one. |
RW | 0 | ||
15 | EFUSE_BLANK | Efuse scanning detected if fuse ROM is blank: 0 : Not blank 1 : Blank |
RO | 0 | ||
14 | EFUSE_TIMEOUT | Efuse scanning resulted in timeout error. 0 : No Timeout error 1 : Timeout Error |
RO | 0 | ||
13 | SPRS_BYTE_NOT_OK | Efuse scanning resulted in scan chain Sparse byte error. 0 : No Sparse error 1 : Sparse Error |
RO | 0 | ||
12:8 | EFUSE_ERRCODE | Same as EFUSEERROR.CODE | RO | 0b0 0000 | ||
7:6 | RESERVED7 | Software should not rely on the value of a reserved bit. To provide compatibility with future products, the value of a reserved bit should be preserved across a read-modify-write operation | RO | 0b00 | ||
5:4 | BUSY | NW FW_SMSTAT.CMD_IN_PROGRESS bit. This flag is valid immediately after the operation setting it 0 : Not busy 1 : Busy Bit 4 is for the busy state for Bank0 which is at logical address 0x0 Bit 5 for Bank1. |
RO | 0b00 | ||
3 | READY1T | 1T access readiness status indicator from NW. Comes later than 2T readiness. 1: FLASH banks are ready for 1T accesses 0: FLASH banks are not ready for 1T accesses |
RO | 0 | ||
2 | READY2T | 2T access readiness status indicator from NW 1: FLASH banks are ready for 2T accesses 0: FLASH banks are not ready for 2T accesses |
RO | 0 | ||
1:0 | POWER_MODE | Power state of each of the 2 flash arbiter FSM instances in the flash sub-system. For Thor, these bits should mostly be in the same state since both banks are in the same power mode. 0 : Active 1 : Ready for Low power (The 2T readiness has gone low or the flash_off_req has been set=1, and flash_off_ack is ready to be asserted). Bit 0 is for the power state for Bank0 which is at logical address 0x0 Bit 1 for Bank1 |
RO | 0b00 |
Address Offset | 0x0000 0024 | ||
Physical Address | 0x5803 0024 | Instance | 0x5803 0024 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31 | RESERVED31 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
30 | DIS_FWTEST | Internal. Only to be used through TI provided API. | RW | 0 | ||
29:12 | RESERVED12 | Internal. Only to be used through TI provided API. | RO | 0b00 0000 0000 0000 0000 | ||
11 | MAIN_STICKY_EN | Internal. Only to be used through TI provided API. | RW | 0 | ||
10 | CCFG_STICKY_EN | Internal. Only to be used through TI provided API. | RW | 0 | ||
9 | FCFG_STICKY_EN | Internal. Only to be used through TI provided API. | RW | 0 | ||
8 | ENGR_TRIM_STICKY_EN | Internal. Only to be used through TI provided API. | RW | 0 | ||
7:6 | RESERVED6 | Internal. Only to be used through TI provided API. | RO | 0b00 | ||
5 | DIS_EFUSECLK | Internal. Only to be used through TI provided API. | RW | 0 | ||
4 | DIS_READACCESS | Internal. Only to be used through TI provided API. | RW | 0 | ||
3:1 | RESERVED1 | Internal. Only to be used through TI provided API. | RW | 0b000 | ||
0 | BP_TRIMCFG_EN | Internal. Only to be used through TI provided API. | RW | 0 |
Address Offset | 0x0000 002C | ||
Physical Address | 0x5803 002C | Instance | 0x5803 002C |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:10 | RESERVED10 | Internal. Only to be used through TI provided API. | RO | 0b00 0000 0000 0000 0000 0000 | ||
9:7 | SECTORS | Internal. Only to be used through TI provided API. | RW | 0b100 | ||
6:0 | RESERVED0 | Internal. Only to be used through TI provided API. | RO | 0b000 0000 |
Address Offset | 0x0000 003C | ||
Physical Address | 0x5803 003C | Instance | 0x5803 003C |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:3 | RESERVED3 | Internal. Only to be used through TI provided API. | RO | 0b0 0000 0000 0000 0000 0000 0000 0000 | ||
2:0 | FWLOCK | Internal. Only to be used through TI provided API. | RW | 0b000 |
Address Offset | 0x0000 0040 | ||
Physical Address | 0x5803 0040 | Instance | 0x5803 0040 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:3 | RESERVED3 | Internal. Only to be used through TI provided API. | RO | 0b0 0000 0000 0000 0000 0000 0000 0000 | ||
2:0 | FWFLAG | Internal. Only to be used through TI provided API. | RW | 0b000 |
Address Offset | 0x0000 0050 | ||
Physical Address | 0x5803 0050 | Instance | 0x5803 0050 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | RESERVED32 | Internal. Only to be used through TI provided API. | RW | 0x0000 0000 |
Address Offset | 0x0000 0054 | ||
Physical Address | 0x5803 0054 | Instance | 0x5803 0054 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | RESERVED32 | Internal. Only to be used through TI provided API. | RW | 0x0000 0000 |
Address Offset | 0x0000 0058 | ||
Physical Address | 0x5803 0058 | Instance | 0x5803 0058 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:28 | RESERVED6 | Internal. Only to be used through TI provided API. | RW | 0x0 | ||
27:22 | REDSWSELW3 | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
21:16 | REDSWSELW2 | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
15:10 | REDSWSELW1 | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
9:4 | REDSWSELW0 | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
3 | REDSWENW3 | Internal. Only to be used through TI provided API. | RW | 0 | ||
2 | REDSWENW2 | Internal. Only to be used through TI provided API. | RW | 0 | ||
1 | REDSWENW1 | Internal. Only to be used through TI provided API. | RW | 0 | ||
0 | REDSWENW0 | Internal. Only to be used through TI provided API. | RW | 0 |
Address Offset | 0x0000 005C | ||
Physical Address | 0x5803 005C | Instance | 0x5803 005C |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | BANK0_TRIM_CFG_0 | Internal. Only to be used through TI provided API. | RW | 0x0000 0000 |
Address Offset | 0x0000 0060 | ||
Physical Address | 0x5803 0060 | Instance | 0x5803 0060 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | RESERVED32 | Internal. Only to be used through TI provided API. | RW | 0x0000 0000 |
Address Offset | 0x0000 0064 | ||
Physical Address | 0x5803 0064 | Instance | 0x5803 0064 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | RESERVED32 | Internal. Only to be used through TI provided API. | RW | 0x0000 0000 |
Address Offset | 0x0000 0068 | ||
Physical Address | 0x5803 0068 | Instance | 0x5803 0068 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:28 | RESERVED6 | Internal. Only to be used through TI provided API. | RW | 0x0 | ||
27:22 | REDSWSELW3 | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
21:16 | REDSWSELW2 | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
15:10 | REDSWSELW1 | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
9:4 | REDSWSELW0 | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
3 | REDSWENW3 | Internal. Only to be used through TI provided API. | RW | 0 | ||
2 | REDSWENW2 | Internal. Only to be used through TI provided API. | RW | 0 | ||
1 | REDSWENW1 | Internal. Only to be used through TI provided API. | RW | 0 | ||
0 | REDSWENW0 | Internal. Only to be used through TI provided API. | RW | 0 |
Address Offset | 0x0000 006C | ||
Physical Address | 0x5803 006C | Instance | 0x5803 006C |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | BANK1_TRIM_CFG_0 | Internal. Only to be used through TI provided API. | RW | 0x0000 0000 |
Address Offset | 0x0000 0070 | ||
Physical Address | 0x5803 0070 | Instance | 0x5803 0070 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:26 | RESERVED6 | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
25:20 | VWLCT | Internal. Only to be used through TI provided API. | RW | 0b00 0101 | ||
19:14 | VSLCT | Internal. Only to be used through TI provided API. | RW | 0b01 0110 | ||
13:9 | VREADCT | Internal. Only to be used through TI provided API. | RW | 0b0 1010 | ||
8:4 | VINLOWCCORCT | Internal. Only to be used through TI provided API. | RW | 0b0 0000 | ||
3:0 | VINHICCORCT | Internal. Only to be used through TI provided API. | RW | 0x0 |
Address Offset | 0x0000 0074 | ||
Physical Address | 0x5803 0074 | Instance | 0x5803 0074 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31 | VINHICCORCTLSB | Internal. Only to be used through TI provided API. | RW | 0 | ||
30:25 | VINHCT | Internal. Only to be used through TI provided API. | RW | 0b00 1100 | ||
24:20 | VCGCT | Internal. Only to be used through TI provided API. | RW | 0b1 0010 | ||
19:15 | IREFVRDCT | Internal. Only to be used through TI provided API. | RW | 0b0 0000 | ||
14:10 | IREFTCCT | Internal. Only to be used through TI provided API. | RW | 0b0 0000 | ||
9:6 | IREFCT | Internal. Only to be used through TI provided API. | RW | 0x0 | ||
5:0 | FOSCCT | Internal. Only to be used through TI provided API. | RW | 0b00 0000 |
Address Offset | 0x0000 0078 | ||
Physical Address | 0x5803 0078 | Instance | 0x5803 0078 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:30 | RESERVED2 | Internal. Only to be used through TI provided API. | RW | 0b00 | ||
29:20 | VHVCT_PV | Internal. Only to be used through TI provided API. | RW | 0b00 0000 1011 | ||
19:10 | VHVCT_PGM | Internal. Only to be used through TI provided API. | RW | 0b01 0011 0001 | ||
9:0 | VHVCT_ERS | Internal. Only to be used through TI provided API. | RW | 0b01 0011 1010 |
Address Offset | 0x0000 1000 | ||
Physical Address | 0x5803 1000 | Instance | 0x5803 1000 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:29 | RESERVED29 | Internal. Only to be used through TI provided API. | RO | 0b000 | ||
28:24 | INSTRUCTION | Internal. Only to be used through TI provided API. | RW | 0b0 0000 | ||
23:16 | RESERVED16 | Internal. Only to be used through TI provided API. | RO | 0x00 | ||
15:0 | DUMPWORD | Internal. Only to be used through TI provided API. | RW | 0x0000 |
Address Offset | 0x0000 1004 | ||
Physical Address | 0x5803 1004 | Instance | 0x5803 1004 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:16 | RESERVED16 | Internal. Only to be used through TI provided API. | RO | 0x0000 | ||
15:11 | BLOCK | Internal. Only to be used through TI provided API. | RW | 0b0 0000 | ||
10:0 | ROW | Internal. Only to be used through TI provided API. | RW | 0b000 0000 0000 |
Address Offset | 0x0000 1008 | ||
Physical Address | 0x5803 1008 | Instance | 0x5803 1008 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Internal. Only to be used through TI provided API. | RO | 0x00 0000 | ||
7:3 | SPARE | Internal. Only to be used through TI provided API. | RW | 0b0 0000 | ||
2 | P | Internal. Only to be used through TI provided API. | RW | 0 | ||
1 | R | Internal. Only to be used through TI provided API. | RW | 0 | ||
0 | EEN | Internal. Only to be used through TI provided API. | RW | 0 |
Address Offset | 0x0000 100C | ||
Physical Address | 0x5803 100C | Instance | 0x5803 100C |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | DATA | Internal. Only to be used through TI provided API. | RW | 0x0000 0000 |
Address Offset | 0x0000 1010 | ||
Physical Address | 0x5803 1010 | Instance | 0x5803 1010 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:9 | RESERVED9 | Internal. Only to be used through TI provided API. | RO | 0b000 0000 0000 0000 0000 0000 | ||
8 | IDLEGATING | Internal. Only to be used through TI provided API. | RW | 0 | ||
7:5 | RESERVED5 | Internal. Only to be used through TI provided API. | RO | 0b000 | ||
4:3 | SLAVEPOWER | Internal. Only to be used through TI provided API. | RW | 0b00 | ||
2:1 | RESERVED1 | Internal. Only to be used through TI provided API. | RO | 0b00 | ||
0 | GATING | Internal. Only to be used through TI provided API. | RW | 1 |
Address Offset | 0x0000 1014 | ||
Physical Address | 0x5803 1014 | Instance | 0x5803 1014 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:1 | RESERVED1 | Internal. Only to be used through TI provided API. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | RESETDONE | Internal. Only to be used through TI provided API. | RO | 1 |
Address Offset | 0x0000 1018 | ||
Physical Address | 0x5803 1018 | Instance | 0x5803 1018 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:24 | RESERVED24 | Internal. Only to be used through TI provided API. | RO | 0x00 | ||
23:0 | ACCUMULATOR | Internal. Only to be used through TI provided API. | RO | 0x00 0000 |
Address Offset | 0x0000 101C | ||
Physical Address | 0x5803 101C | Instance | 0x5803 101C |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:24 | RESERVED24 | Internal. Only to be used through TI provided API. | RO | 0x00 | ||
23 | DISROW0 | Internal. Only to be used through TI provided API. | RW | 0 | ||
22 | SPARE | Internal. Only to be used through TI provided API. | RW | 0 | ||
21 | EFC_SELF_TEST_ERROR | Internal. Only to be used through TI provided API. | RW | 0 | ||
20 | EFC_INSTRUCTION_INFO | Internal. Only to be used through TI provided API. | RW | 0 | ||
19 | EFC_INSTRUCTION_ERROR | Internal. Only to be used through TI provided API. | RW | 0 | ||
18 | EFC_AUTOLOAD_ERROR | Internal. Only to be used through TI provided API. | RW | 0 | ||
17:14 | OUTPUTENABLE | Internal. Only to be used through TI provided API. | RW | 0x0 | ||
13 | SYS_ECC_SELF_TEST_EN | Internal. Only to be used through TI provided API. | RW | 0 | ||
12 | SYS_ECC_OVERRIDE_EN | Internal. Only to be used through TI provided API. | RW | 0 | ||
11 | EFC_FDI | Internal. Only to be used through TI provided API. | RW | 0 | ||
10 | SYS_DIEID_AUTOLOAD_EN | Internal. Only to be used through TI provided API. | RW | 0 | ||
9:8 | SYS_REPAIR_EN | Internal. Only to be used through TI provided API. | RW | 0b00 | ||
7:4 | SYS_WS_READ_STATES | Internal. Only to be used through TI provided API. | RW | 0x0 | ||
3:0 | INPUTENABLE | Internal. Only to be used through TI provided API. | RW | 0x0 |
Address Offset | 0x0000 1020 | ||
Physical Address | 0x5803 1020 | Instance | 0x5803 1020 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:1 | RESERVED1 | Internal. Only to be used through TI provided API. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | KEY | Internal. Only to be used through TI provided API. | RO | 0 |
Address Offset | 0x0000 1024 | ||
Physical Address | 0x5803 1024 | Instance | 0x5803 1024 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | CODE | Internal. Only to be used through TI provided API. | RW | 0x0000 0000 |
Address Offset | 0x0000 1028 | ||
Physical Address | 0x5803 1028 | Instance | 0x5803 1028 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:25 | ODPYEAR | Internal. Only to be used through TI provided API. | RO | 0xXX | ||
24:21 | ODPMONTH | Internal. Only to be used through TI provided API. | RO | 0xX | ||
20:16 | ODPDAY | Internal. Only to be used through TI provided API. | RO | 0xXX | ||
15:9 | EFUSEYEAR | Internal. Only to be used through TI provided API. | RO | 0xXX | ||
8:5 | EFUSEMONTH | Internal. Only to be used through TI provided API. | RO | 0xX | ||
4:0 | EFUSEDAY | Internal. Only to be used through TI provided API. | RO | 0xXX |
Address Offset | 0x0000 102C | ||
Physical Address | 0x5803 102C | Instance | 0x5803 102C |
Description | Internal. Only to be used through TI provided API. | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:16 | RESERVED16 | Internal. Only to be used through TI provided API. | RO | 0x0000 | ||
15 | EFC_SELF_TEST_DONE | Internal. Only to be used through TI provided API. | RO | X | ||
14 | EFC_SELF_TEST_ERROR | Internal. Only to be used through TI provided API. | RO | X | ||
13 | SYS_ECC_SELF_TEST_EN | Internal. Only to be used through TI provided API. | RO | X | ||
12 | EFC_INSTRUCTION_INFO | Internal. Only to be used through TI provided API. | RO | X | ||
11 | EFC_INSTRUCTION_ERROR | Internal. Only to be used through TI provided API. | RO | X | ||
10 | EFC_AUTOLOAD_ERROR | Internal. Only to be used through TI provided API. | RO | X | ||
9 | SYS_ECC_OVERRIDE_EN | Internal. Only to be used through TI provided API. | RO | X | ||
8 | EFC_READY | Internal. Only to be used through TI provided API. | RO | X | ||
7 | EFC_FCLRZ | Internal. Only to be used through TI provided API. | RO | X | ||
6 | SYS_DIEID_AUTOLOAD_EN | Internal. Only to be used through TI provided API. | RO | X | ||
5:4 | SYS_REPAIR_EN | Internal. Only to be used through TI provided API. | RO | 0xX | ||
3:0 | SYS_WS_READ_STATES | Internal. Only to be used through TI provided API. | RO | 0xX |
Address Offset | 0x0000 1030 | ||
Physical Address | 0x5803 1030 | Instance | 0x5803 1030 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:6 | RESERVED6 | Internal. Only to be used through TI provided API. | RO | 0b00 0000 0000 0000 0000 0000 0000 | ||
5:0 | DATA | Internal. Only to be used through TI provided API. | RW | 0b00 0000 |
Address Offset | 0x0000 1034 | ||
Physical Address | 0x5803 1034 | Instance | 0x5803 1034 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:10 | RESERVED10 | Internal. Only to be used through TI provided API. | RO | 0b00 0000 0000 0000 0000 0000 | ||
9:8 | DATABIT | Internal. Only to be used through TI provided API. | RW | 0b00 | ||
7:4 | READCLOCK | Internal. Only to be used through TI provided API. | RW | 0x0 | ||
3 | DEBUG | Internal. Only to be used through TI provided API. | RW | 0 | ||
2 | SPARE | Internal. Only to be used through TI provided API. | RW | 0 | ||
1:0 | MARGIN | Internal. Only to be used through TI provided API. | RW | 0b00 |
Address Offset | 0x0000 1038 | ||
Physical Address | 0x5803 1038 | Instance | 0x5803 1038 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31 | RESERVED31 | Internal. Only to be used through TI provided API. | RO | 0 | ||
30 | COMPAREDISABLE | Internal. Only to be used through TI provided API. | RW | 0 | ||
29:14 | CLOCKSTALL | Internal. Only to be used through TI provided API. | RW | 0x0000 | ||
13 | VPPTOVDD | Internal. Only to be used through TI provided API. | RW | 0 | ||
12:9 | ITERATIONS | Internal. Only to be used through TI provided API. | RW | 0x0 | ||
8:0 | WRITECLOCK | Internal. Only to be used through TI provided API. | RW | 0b0 0000 0000 |
Address Offset | 0x0000 103C | ||
Physical Address | 0x5803 103C | Instance | 0x5803 103C |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:6 | RESERVED6 | Internal. Only to be used through TI provided API. | RO | 0b00 0000 0000 0000 0000 0000 0000 | ||
5 | DONE | Internal. Only to be used through TI provided API. | RW | 0 | ||
4:0 | CODE | Internal. Only to be used through TI provided API. | RW | 0b0 0000 |
Address Offset | 0x0000 1040 | ||
Physical Address | 0x5803 1040 | Instance | 0x5803 1040 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:1 | FROMN | Internal. Only to be used through TI provided API. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | FROM0 | Internal. Only to be used through TI provided API. | RO | 0 |
Address Offset | 0x0000 1044 | ||
Physical Address | 0x5803 1044 | Instance | 0x5803 1044 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:1 | FROMN | Internal. Only to be used through TI provided API. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | FROM0 | Internal. Only to be used through TI provided API. | RO | 0 |
Address Offset | 0x0000 1048 | ||
Physical Address | 0x5803 1048 | Instance | 0x5803 1048 |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | CYCLES | Internal. Only to be used through TI provided API. | RW | 0x0000 0000 |
Address Offset | 0x0000 104C | ||
Physical Address | 0x5803 104C | Instance | 0x5803 104C |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | SIGNATURE | Internal. Only to be used through TI provided API. | RW | 0x0000 0000 |
© 2015 - 2016. Texas Instruments | All Rights Reserved |