Instance: CPU_SAU
Component: CPU_SAU
Base address: 0xE000EDD0
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
RW |
32 |
0x0000 0000 |
0x0000 0000 |
0xE000 EDD0 |
|
RW |
32 |
0x0000 0000 |
0x0000 0004 |
0xE000 EDD4 |
|
RW |
32 |
0x0000 0000 |
0x0000 0008 |
0xE000 EDD8 |
|
RW |
32 |
0x0000 0000 |
0x0000 000C |
0xE000 EDDC |
|
RW |
32 |
0x0000 0000 |
0x0000 0010 |
0xE000 EDE0 |
|
RW |
32 |
0x0000 0000 |
0x0000 0014 |
0xE000 EDE4 |
|
RW |
32 |
0x0000 0000 |
0x0000 0018 |
0xE000 EDE8 |
Address Offset | 0x0000 0000 | ||
Physical Address | 0xE000 EDD0 | Instance | 0xE000 EDD0 |
Description | Allows enabling of the Security Attribution Unit | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 0000 | ||
1 | ALLNS | When SAU_CTRL.ENABLE is 0 this bit controls if the memory is marked as Non-secure or Secure | RW | 0 | ||
0 | ENABLE | Enables the SAU | RW | 0 |
Address Offset | 0x0000 0004 | ||
Physical Address | 0xE000 EDD4 | Instance | 0xE000 EDD4 |
Description | Indicates the number of regions implemented by the Security Attribution Unit | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:0 | SREGION | The number of implemented SAU regions | RO | 0x00 |
Address Offset | 0x0000 0008 | ||
Physical Address | 0xE000 EDD8 | Instance | 0xE000 EDD8 |
Description | Selects the region currently accessed by SAU_RBAR and SAU_RLAR | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:0 | REGION | Indicates the SAU region accessed by SAU_RBAR and SAU_RLAR | RW | 0x00 |
Address Offset | 0x0000 000C | ||
Physical Address | 0xE000 EDDC | Instance | 0xE000 EDDC |
Description | Provides indirect read and write access to the base address of the currently selected SAU region | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:5 | BADDR | Holds bits [31:5] of the base address for the selected SAU region | RW | 0b000 0000 0000 0000 0000 0000 0000 | ||
4:0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b0 0000 |
Address Offset | 0x0000 0010 | ||
Physical Address | 0xE000 EDE0 | Instance | 0xE000 EDE0 |
Description | Provides indirect read and write access to the limit address of the currently selected SAU region | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:5 | LADDR | Holds bits [31:5] of the limit address for the selected SAU region | RW | 0b000 0000 0000 0000 0000 0000 0000 | ||
4:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 | ||
1 | NSC | Controls whether Non-secure state is permitted to execute an SG instruction from this region | RW | 0 | ||
0 | ENABLE | SAU region enable | RW | 0 |
Address Offset | 0x0000 0014 | ||
Physical Address | 0xE000 EDE4 | Instance | 0xE000 EDE4 |
Description | Provides information about any security related faults | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7 | LSERR | Sticky flag indicating that an error occurred during lazy state activation or deactivation | RW | 0 | ||
6 | SFARVALID | This bit is set when the SFAR register contains a valid value. As with similar fields, such as BFSR.BFARVALID and MMFSR.MMARVALID, this bit can be cleared by other exceptions, such as BusFault | RW | 0 | ||
5 | LSPERR | Stick flag indicating that an SAU or IDAU violation occurred during the lazy preservation of floating-point state | RW | 0 | ||
4 | INVTRAN | Sticky flag indicating that an exception was raised due to a branch that was not flagged as being domain crossing causing a transition from Secure to Non-secure memory | RW | 0 | ||
3 | AUVIOL | Sticky flag indicating that an attempt was made to access parts of the address space that are marked as Secure with NS-Req for the transaction set to Non-secure. This bit is not set if the violation occurred during lazy state preservation. See LSPERR | RW | 0 | ||
2 | INVER | This can be caused by EXC_RETURN.DCRS being set to 0 when returning from an exception in the Non-secure state, or by EXC_RETURN.ES being set to 1 when returning from an exception in the Non-secure state | RW | 0 | ||
1 | INVIS | This bit is set if the integrity signature in an exception stack frame is found to be invalid during the unstacking operation | RW | 0 | ||
0 | INVEP | This bit is set if a function call from the Non-secure state or exception targets a non-SG instruction in the Secure state. This bit is also set if the target address is a SG instruction, but there is no matching SAU/IDAU region with the NSC flag set | RW | 0 |
Address Offset | 0x0000 0018 | ||
Physical Address | 0xE000 EDE8 | Instance | 0xE000 EDE8 |
Description | Shows the address of the memory location that caused a Security violation | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | ADDRESS | The address of an access that caused a attribution unit violation. This field is only valid when SFSR.SFARVALID is set. This allows the actual flip flops associated with this register to be shared with other fault address registers. If an implementation chooses to share the storage in this way, care must be taken to not leak Secure address information to the Non-secure state. One way of achieving this is to share the SFAR register with the MMFAR_S register, which is not accessible to the Non-secure state | RW | 0x0000 0000 |
© 2015 - 2016. Texas Instruments | All Rights Reserved |