Instance: CPU_CTI
Component: CPU_CTI
Base address: 0xE0042000
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
RW |
32 |
0x0000 0000 |
0x0000 0000 |
0xE004 2000 |
|
RW |
32 |
0x0000 0000 |
0x0000 0010 |
0xE004 2010 |
|
RW |
32 |
0x0000 0000 |
0x0000 0014 |
0xE004 2014 |
|
RW |
32 |
0x0000 0000 |
0x0000 0018 |
0xE004 2018 |
|
RW |
32 |
0x0000 0000 |
0x0000 001C |
0xE004 201C |
|
RW |
32 |
0x0000 0000 |
0x0000 0020 |
0xE004 2020 |
|
RW |
32 |
0x0000 0000 |
0x0000 0024 |
0xE004 2024 |
|
RW |
32 |
0x0000 0000 |
0x0000 0028 |
0xE004 2028 |
|
RW |
32 |
0x0000 0000 |
0x0000 002C |
0xE004 202C |
|
RW |
32 |
0x0000 0000 |
0x0000 0030 |
0xE004 2030 |
|
RW |
32 |
0x0000 0000 |
0x0000 0034 |
0xE004 2034 |
|
RW |
32 |
0x0000 0000 |
0x0000 0038 |
0xE004 2038 |
|
RW |
32 |
0x0000 0000 |
0x0000 003C |
0xE004 203C |
|
RW |
32 |
0x0000 0000 |
0x0000 00A0 |
0xE004 20A0 |
|
RW |
32 |
0x0000 0000 |
0x0000 00A4 |
0xE004 20A4 |
|
RW |
32 |
0x0000 0000 |
0x0000 00A8 |
0xE004 20A8 |
|
RW |
32 |
0x0000 0000 |
0x0000 00AC |
0xE004 20AC |
|
RW |
32 |
0x0000 0000 |
0x0000 00B0 |
0xE004 20B0 |
|
RW |
32 |
0x0000 0000 |
0x0000 00B4 |
0xE004 20B4 |
|
RW |
32 |
0x0000 0000 |
0x0000 00B8 |
0xE004 20B8 |
|
RW |
32 |
0x0000 0000 |
0x0000 00BC |
0xE004 20BC |
|
RW |
32 |
0x0000 0000 |
0x0000 0130 |
0xE004 2130 |
|
RW |
32 |
0x0000 0000 |
0x0000 0134 |
0xE004 2134 |
|
RW |
32 |
0x0000 0000 |
0x0000 0138 |
0xE004 2138 |
|
RW |
32 |
0x0000 0000 |
0x0000 0140 |
0xE004 2140 |
|
RW |
32 |
0x0000 0000 |
0x0000 0144 |
0xE004 2144 |
|
RW |
32 |
0x0000 0000 |
0x0000 0EE4 |
0xE004 2EE4 |
|
RW |
32 |
0x0000 0000 |
0x0000 0EE8 |
0xE004 2EE8 |
|
RW |
32 |
0x0000 0000 |
0x0000 0EF4 |
0xE004 2EF4 |
|
RW |
32 |
0x0000 0000 |
0x0000 0F00 |
0xE004 2F00 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FBC |
0xE004 2FBC |
|
RW |
32 |
0x0000 0000 |
0x0000 0FC8 |
0xE004 2FC8 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FCC |
0xE004 2FCC |
|
RW |
32 |
0x0000 0000 |
0x0000 0FD0 |
0xE004 2FD0 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FD4 |
0xE004 2FD4 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FD8 |
0xE004 2FD8 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FDC |
0xE004 2FDC |
|
RW |
32 |
0x0000 0000 |
0x0000 0FE0 |
0xE004 2FE0 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FE4 |
0xE004 2FE4 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FE8 |
0xE004 2FE8 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FEC |
0xE004 2FEC |
|
RW |
32 |
0x0000 0000 |
0x0000 0FF0 |
0xE004 2FF0 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FF4 |
0xE004 2FF4 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FF8 |
0xE004 2FF8 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FFC |
0xE004 2FFC |
Address Offset | 0x0000 0000 | ||
Physical Address | 0xE004 2000 | Instance | 0xE004 2000 |
Description | CTI Control Register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | GLBEN | Enables or disables the CTI. | RW | 0 |
Address Offset | 0x0000 0010 | ||
Physical Address | 0xE004 2010 | Instance | 0xE004 2010 |
Description | CTI Interrupt Acknowledge Register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:0 | INTACK | Acknowledges the corresponding ctitrigout output. There is one bit of the register for each ctitrigout output. When a 1 is written to a bit in this register, the corresponding ctitrigout is acknowledged, causing it to be cleared | WO | 0x00 |
Address Offset | 0x0000 0014 | ||
Physical Address | 0xE004 2014 | Instance | 0xE004 2014 |
Description | CTI Application Trigger Set Register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | APPSET | Setting a bit HIGH generates a channel event for the selected channel. There is one bit of the register for each channel. Reads as follows: 0 Application trigger is inactive. 1 Application trigger is active. Writes as follows: 0 No effect. 1 Generate channel event. | RW | 0x0 |
Address Offset | 0x0000 0018 | ||
Physical Address | 0xE004 2018 | Instance | 0xE004 2018 |
Description | CTI Application Trigger Clear Register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | APPCLEAR | Sets the corresponding bits in the CTIAPPSET to 0. There is one bit of the register for each channel.On writes, for each bit: 0 Has no effect. 1 Clears the corresponding channel event.Setting a bit HIGH generates a channel event for the selected channel. There is one bit of the register for each channel. Reads as follows: 0 Application trigger is inactive. 1 Application trigger is active. Writes as follows: 0 No effect. 1 Generate channel event. | RW | 0x0 |
Address Offset | 0x0000 001C | ||
Physical Address | 0xE004 201C | Instance | 0xE004 201C |
Description | CTI Application Pulse Register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | APPULSE | Setting a bit HIGH generates a channel event pulse for the selected channel. There is one bit of the register for each channel. On writes, for each bit: 0 Has no effect. 1 Generate an event pulse on the corresponding channel. | WO | 0x0 |
Address Offset | 0x0000 0020 | ||
Physical Address | 0xE004 2020 | Instance | 0xE004 2020 |
Description | CTI Trigger to Channel Enable Registers | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | TRIGINEN | Enables a cross trigger event to the corresponding channel when a ctitrigin input is activated. There is one bit of the field for each of the four channels. On writes, for each bit: 0 Input trigger 0 events are ignored by the corresponding channel. 1 When an event is received on input trigger 0, ctitrigin[0], generate an event on the channel corresponding to this bit. | RW | 0x0 |
Address Offset | 0x0000 0024 | ||
Physical Address | 0xE004 2024 | Instance | 0xE004 2024 |
Description | CTI Trigger to Channel Enable Registers | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | TRIGINEN | Enables a cross trigger event to the corresponding channel when a ctitrigin input is activated. There is one bit of the field for each of the four channels. On writes, for each bit: 0 Input trigger 1 events are ignored by the corresponding channel. 1 When an event is received on input trigger 1, ctitrigin[1], generate an event on the channel corresponding to this bit. | RW | 0x0 |
Address Offset | 0x0000 0028 | ||
Physical Address | 0xE004 2028 | Instance | 0xE004 2028 |
Description | CTI Trigger to Channel Enable Registers | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | TRIGINEN | Enables a cross trigger event to the corresponding channel when a ctitrigin input is activated. There is one bit of the field for each of the four channels. On writes, for each bit: 0 Input trigger 2 events are ignored by the corresponding channel. 1 When an event is received on input trigger 2, ctitrigin[2], generate an event on the channel corresponding to this bit. | RW | 0x0 |
Address Offset | 0x0000 002C | ||
Physical Address | 0xE004 202C | Instance | 0xE004 202C |
Description | CTI Trigger to Channel Enable Registers | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | TRIGINEN | Enables a cross trigger event to the corresponding channel when a ctitrigin input is activated. There is one bit of the field for each of the four channels. On writes, for each bit: 0 Input trigger 3 events are ignored by the corresponding channel. 1 When an event is received on input trigger 3, ctitrigin[3], generate an event on the channel corresponding to this bit. | RW | 0x0 |
Address Offset | 0x0000 0030 | ||
Physical Address | 0xE004 2030 | Instance | 0xE004 2030 |
Description | CTI Trigger to Channel Enable Registers | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | TRIGINEN | Enables a cross trigger event to the corresponding channel when a ctitrigin input is activated. There is one bit of the field for each of the four channels. On writes, for each bit: 0 Input trigger 4 events are ignored by the corresponding channel. 1 When an event is received on input trigger 4, ctitrigin[4], generate an event on the channel corresponding to this bit. | RW | 0x0 |
Address Offset | 0x0000 0034 | ||
Physical Address | 0xE004 2034 | Instance | 0xE004 2034 |
Description | CTI Trigger to Channel Enable Registers | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | TRIGINEN | Enables a cross trigger event to the corresponding channel when a ctitrigin input is activated. There is one bit of the field for each of the four channels. On writes, for each bit: 0 Input trigger 5 events are ignored by the corresponding channel. 1 When an event is received on input trigger 5, ctitrigin[5], generate an event on the channel corresponding to this bit. | RW | 0x0 |
Address Offset | 0x0000 0038 | ||
Physical Address | 0xE004 2038 | Instance | 0xE004 2038 |
Description | CTI Trigger to Channel Enable Registers | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | TRIGINEN | Enables a cross trigger event to the corresponding channel when a ctitrigin input is activated. There is one bit of the field for each of the four channels. On writes, for each bit: 0 Input trigger 6 events are ignored by the corresponding channel. 1 When an event is received on input trigger 6, ctitrigin[6], generate an event on the channel corresponding to this bit. | RW | 0x0 |
Address Offset | 0x0000 003C | ||
Physical Address | 0xE004 203C | Instance | 0xE004 203C |
Description | CTI Trigger to Channel Enable Registers | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | TRIGINEN | Enables a cross trigger event to the corresponding channel when a ctitrigin input is activated. There is one bit of the field for each of the four channels. On writes, for each bit: 0 Input trigger 7 events are ignored by the corresponding channel. 1 When an event is received on input trigger 7, ctitrigin[7], generate an event on the channel corresponding to this bit. | RW | 0x0 |
Address Offset | 0x0000 00A0 | ||
Physical Address | 0xE004 20A0 | Instance | 0xE004 20A0 |
Description | CTI Trigger to Channel Enable Registers | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | TRIGOUTEN | Enables a cross trigger event to ctitrigout when the corresponding channel is activated. There is one bit of the field for each of the four channels. On writes, for each bit 0 The corresponding channel is ignored by the output trigger 0. 1 When an event occurs on the channel corresponding to this bit, generate an event on output event 0, ctitrigout[0]. | RW | 0x0 |
Address Offset | 0x0000 00A4 | ||
Physical Address | 0xE004 20A4 | Instance | 0xE004 20A4 |
Description | CTI Trigger to Channel Enable Registers | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | TRIGOUTEN | Enables a cross trigger event to ctitrigout when the corresponding channel is activated. There is one bit of the field for each of the four channels. On writes, for each bit 0 The corresponding channel is ignored by the output trigger 1. 1 When an event occurs on the channel corresponding to this bit, generate an event on output event 1, ctitrigout[1]. | RW | 0x0 |
Address Offset | 0x0000 00A8 | ||
Physical Address | 0xE004 20A8 | Instance | 0xE004 20A8 |
Description | CTI Trigger to Channel Enable Registers | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | TRIGOUTEN | Enables a cross trigger event to ctitrigout when the corresponding channel is activated. There is one bit of the field for each of the four channels. On writes, for each bit 0 The corresponding channel is ignored by the output trigger 2. 1 When an event occurs on the channel corresponding to this bit, generate an event on output event 2, ctitrigout[2]. | RW | 0x0 |
Address Offset | 0x0000 00AC | ||
Physical Address | 0xE004 20AC | Instance | 0xE004 20AC |
Description | CTI Trigger to Channel Enable Registers | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | TRIGOUTEN | Enables a cross trigger event to ctitrigout when the corresponding channel is activated. There is one bit of the field for each of the four channels. On writes, for each bit 0 The corresponding channel is ignored by the output trigger 3. 1 When an event occurs on the channel corresponding to this bit, generate an event on output event 3, ctitrigout[3]. | RW | 0x0 |
Address Offset | 0x0000 00B0 | ||
Physical Address | 0xE004 20B0 | Instance | 0xE004 20B0 |
Description | CTI Trigger to Channel Enable Registers | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | TRIGOUTEN | Enables a cross trigger event to ctitrigout when the corresponding channel is activated. There is one bit of the field for each of the four channels. On writes, for each bit 0 The corresponding channel is ignored by the output trigger 4. 1 When an event occurs on the channel corresponding to this bit, generate an event on output event 4, ctitrigout[4]. | RW | 0x0 |
Address Offset | 0x0000 00B4 | ||
Physical Address | 0xE004 20B4 | Instance | 0xE004 20B4 |
Description | CTI Trigger to Channel Enable Registers | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | TRIGOUTEN | Enables a cross trigger event to ctitrigout when the corresponding channel is activated. There is one bit of the field for each of the four channels. On writes, for each bit 0 The corresponding channel is ignored by the output trigger 5. 1 When an event occurs on the channel corresponding to this bit, generate an event on output event 5, ctitrigout[5]. | RW | 0x0 |
Address Offset | 0x0000 00B8 | ||
Physical Address | 0xE004 20B8 | Instance | 0xE004 20B8 |
Description | CTI Trigger to Channel Enable Registers | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | TRIGOUTEN | Enables a cross trigger event to ctitrigout when the corresponding channel is activated. There is one bit of the field for each of the four channels. On writes, for each bit 0 The corresponding channel is ignored by the output trigger 6. 1 When an event occurs on the channel corresponding to this bit, generate an event on output event 6, ctitrigout[6]. | RW | 0x0 |
Address Offset | 0x0000 00BC | ||
Physical Address | 0xE004 20BC | Instance | 0xE004 20BC |
Description | CTI Trigger to Channel Enable Registers | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | TRIGOUTEN | Enables a cross trigger event to ctitrigout when the corresponding channel is activated. There is one bit of the field for each of the four channels. On writes, for each bit 0 The corresponding channel is ignored by the output trigger 7. 1 When an event occurs on the channel corresponding to this bit, generate an event on output event 7, ctitrigout[7]. | RW | 0x0 |
Address Offset | 0x0000 0130 | ||
Physical Address | 0xE004 2130 | Instance | 0xE004 2130 |
Description | CTI Trigger to Channel Enable Registers | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:0 | TRIGINSTATUS | Shows the status of the ctitrigin inputs. There is one bit of the field for each trigger input.Because the register provides a view of the raw ctitrigin inputs, the reset value is UNKNOWN. 1 ctitrigin is active. 0 ctitrigin is inactive | RO | 0x00 |
Address Offset | 0x0000 0134 | ||
Physical Address | 0xE004 2134 | Instance | 0xE004 2134 |
Description | CTI Trigger In Status Register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:0 | TRIGOUTSTATUS | Shows the status of the ctitrigout outputs. There is one bit of the field for each trigger output. 1 ctitrigout is active. 0 ctitrigout is inactive. | RO | 0x00 |
Address Offset | 0x0000 0138 | ||
Physical Address | 0xE004 2138 | Instance | 0xE004 2138 |
Description | CTI Channel In Status Register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | CTICHINSTATUS | Shows the status of the ctichin inputs. There is one bit of the field for each channel input.Because the register provides a view of the raw ctichin inputs, the reset value is UNKNOWN. 0 ctichin is inactive. 1 ctichin is active. | RO | 0x0 |
Address Offset | 0x0000 0140 | ||
Physical Address | 0xE004 2140 | Instance | 0xE004 2140 |
Description | Enable CTI Channel Gate register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3 | CTIGATEEN3 | Enable ctichout3. Set to 0 to disable channel propagation. | RW | 0 | ||
2 | CTIGATEEN2 | Enable ctichout2. Set to 0 to disable channel propagation. | RW | 0 | ||
1 | CTIGATEEN1 | Enable ctichout1. Set to 0 to disable channel propagation. | RW | 0 | ||
0 | CTIGATEEN0 | Enable ctichout0. Set to 0 to disable channel propagation. | RW | 0 |
Address Offset | 0x0000 0144 | ||
Physical Address | 0xE004 2144 | Instance | 0xE004 2144 |
Description | External Multiplexer Control register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:0 | ASICCTL | When external multiplexing is implemented for trigger signals, then the number of multiplexed signals on each trigger must be shown in the Device ID Register. This is done using a Verilog define EXTMUXNUM | RW | 0x00 |
Address Offset | 0x0000 0EE4 | ||
Physical Address | 0xE004 2EE4 | Instance | 0xE004 2EE4 |
Description | Integration Test Channel Output register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | CTCHOUT | Sets the value of the ctichout outputs | WO | 0x0 |
Address Offset | 0x0000 0EE8 | ||
Physical Address | 0xE004 2EE8 | Instance | 0xE004 2EE8 |
Description | Integration Test Trigger Output register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:0 | CTTRIGOUT | Sets the value of the ctitrigout outputs | WO | 0x00 |
Address Offset | 0x0000 0EF4 | ||
Physical Address | 0xE004 2EF4 | Instance | 0xE004 2EF4 |
Description | Integration Test Channel Input register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | ||
3:0 | CTCHIN | Reads the value of the ctichin inputs | RO | 0x0 |
Address Offset | 0x0000 0F00 | ||
Physical Address | 0xE004 2F00 | Instance | 0xE004 2F00 |
Description | Integration Mode Control register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | IME | Integration Mode Enable. 0 Disable integration mode. 1 Enable integration mode | RW | 0 |
Address Offset | 0x0000 0FBC | ||
Physical Address | 0xE004 2FBC | Instance | 0xE004 2FBC |
Description | Device Architecture register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:21 | ARCHITECT | Indicates the component architect: 0x23B ARM | RO | 0b000 0000 0000 | ||
20 | PRESENT | Indicates whether the DEVARCH register is present: 0x1 Present. | RO | 0 | ||
19:16 | REVISION | Indicates the architecture revision: 0x1 Revision 0. | RO | 0x0 | ||
15:0 | ARCHID | Indicates the component: 0x0A34 CoreSight GPR | RO | 0x0000 |
Address Offset | 0x0000 0FC8 | ||
Physical Address | 0xE004 2FC8 | Instance | 0xE004 2FC8 |
Description | Device Configuration register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:20 | RESERVED20 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 | ||
19:16 | NUMCH | Number of ECT channels available | RO | 0x0 | ||
15:8 | NUMTRIG | Number of ECT triggers available | RO | 0x00 | ||
7:5 | RESERVED5 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 | ||
4:0 | EXTMUXNUM | Indicates the number of multiplexers available on Trigger Inputs and Trigger Outputs that are using asicctl. The default value of 0b00000 indicates that no multiplexing is present. This value of this bit depends on the Verilog define EXTMUXNUM that you must change accordingly. | RO | 0b0 0000 |
Address Offset | 0x0000 0FCC | ||
Physical Address | 0xE004 2FCC | Instance | 0xE004 2FCC |
Description | Device Type Identifier register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:4 | SUB | Sub-classification of the type of the debug component as specified in the ARM Architecture Specification within the major classification as specified in the MAJOR field. 0b0001 Indicates that this component is a cross-triggering component | RO | 0x0 | ||
3:0 | MAJOR | Major classification of the type of the debug component as specified in the ARM Architecture Specification for this debug and trace component. 0b0100 Indicates that this component allows a debugger to control other components in a CoreSight SoC-400 system. | RO | 0x0 |
Address Offset | 0x0000 0FD0 | ||
Physical Address | 0xE004 2FD0 | Instance | 0xE004 2FD0 |
Description | CoreSight Periperal ID4 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:4 | SIZE | Always 0b0000. Indicates that the device only occupies 4KB of memory. | RO | 0x0 | ||
3:0 | DES_2 | Together, PIDR1.DES_0, PIDR2.DES_1, and PIDR4.DES_2 identify the designer of the component. 0b0100 JEDEC continuation code. | RO | 0x0 |
Address Offset | 0x0000 0FD4 | ||
Physical Address | 0xE004 2FD4 | Instance | 0xE004 2FD4 |
Description | CoreSight Periperal ID5 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 0000 |
Address Offset | 0x0000 0FD8 | ||
Physical Address | 0xE004 2FD8 | Instance | 0xE004 2FD8 |
Description | CoreSight Periperal ID6 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 0000 |
Address Offset | 0x0000 0FDC | ||
Physical Address | 0xE004 2FDC | Instance | 0xE004 2FDC |
Description | CoreSight Periperal ID7 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 0000 |
Address Offset | 0x0000 0FE0 | ||
Physical Address | 0xE004 2FE0 | Instance | 0xE004 2FE0 |
Description | CoreSight Periperal ID0 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:0 | PART_0 | Bits[7:0] of the 12-bit part number of the component. The designer of the component assigns this part number. 0x06 Indicates bits[7:0] of the part number of the component. | RO | 0x00 |
Address Offset | 0x0000 0FE4 | ||
Physical Address | 0xE004 2FE4 | Instance | 0xE004 2FE4 |
Description | CoreSight Periperal ID1 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:4 | DES_0 | Together, PIDR1.DES_0, PIDR2.DES_1, and PIDR4.DES_2 identify the designer of the component. 0b1011 ARM. Bits[3:0] of the JEDEC JEP106 Identity Code. | RO | 0x0 | ||
3:0 | PART_1 | Bits[11:8] of the 12-bit part number of the component. The designer of the component assigns this part number. 0b1001 Indicates bits[11:8] of the part number of the component. | RO | 0x0 |
Address Offset | 0x0000 0FE8 | ||
Physical Address | 0xE004 2FE8 | Instance | 0xE004 2FE8 |
Description | CoreSight Periperal ID2 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:4 | REVISION | 0b0101 This device is at r1p0. | RO | 0x0 | ||
3 | JEDEC | Always 1. Indicates that the JEDEC-assigned designer ID is used | RO | 0 | ||
2:0 | DES_1 | Together, PIDR1.DES_0, PIDR2.DES_1, and PIDR4.DES_2 identify the designer of the component. 0b011 ARM. Bits[6:4] of the JEDEC JEP106 Identity Code | RO | 0b000 |
Address Offset | 0x0000 0FEC | ||
Physical Address | 0xE004 2FEC | Instance | 0xE004 2FEC |
Description | CoreSight Periperal ID3 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:4 | REVAND | Indicates minor errata fixes specific to the revision of the component being used, for example metal fixes after implementation. In most cases, this field is 0b0000. ARM recommends that the component designers ensure that a metal fix can change this field if required, for example, by driving it from registers that reset to 0b0000. 0b0000 Indicates that there are no errata fixes to this component. | RO | 0x0 | ||
3:0 | CMOD | Customer Modified. Indicates whether the customer has modified the behavior of the component. In most cases, this field is 0b0000. Customers change this value when they make authorized modifications to this component. 0b0000 Indicates that the customer has not modified this component. | RO | 0x0 |
Address Offset | 0x0000 0FF0 | ||
Physical Address | 0xE004 2FF0 | Instance | 0xE004 2FF0 |
Description | CoreSight Component ID0 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:0 | PRMBL_0 | Preamble[0]. Contains bits[7:0] of the component identification code. 0x0D Bits[7:0] of the identification code. | RO | 0x00 |
Address Offset | 0x0000 0FF4 | ||
Physical Address | 0xE004 2FF4 | Instance | 0xE004 2FF4 |
Description | CoreSight Component ID1 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:4 | CLASS | Class of the component, for example, whether the component is a ROM table or a generic CoreSight component. Contains bits[15:12] of the component identification code. 0b1001 Indicates that the component is a CoreSight component. | RO | 0x0 | ||
3:0 | PRMBL_1 | Preamble[1]. Contains bits[11:8] of the component identification code. 0b0000 Bits[11:8] of the identification code. | RO | 0x0 |
Address Offset | 0x0000 0FF8 | ||
Physical Address | 0xE004 2FF8 | Instance | 0xE004 2FF8 |
Description | CoreSight Component ID2 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:0 | PRMBL_2 | Preamble[2]. Contains bits[23:16] of the component identification code. 0x05 Bits[23:16] of the identification code. | RO | 0x00 |
Address Offset | 0x0000 0FFC | ||
Physical Address | 0xE004 2FFC | Instance | 0xE004 2FFC |
Description | CoreSight Component ID3 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:0 | PRMBL_3 | Preamble[3]. Contains bits[31:24] of the component identification code. 0xB1 Bits[31:24] of the identification code. | RO | 0x00 |
© 2015 - 2016. Texas Instruments | All Rights Reserved |