#include <ti/sysbios/heaps/HeapMin.h>
§ iheap
IHeap_Object HeapMin_Struct::iheap |
§ objElem
§ remainSize
size_t HeapMin_Struct::remainSize |
§ startSize
size_t HeapMin_Struct::startSize |
§ buf
char* HeapMin_Struct::buf |
Buffer that will be managed by the heap instance.
When creating a heap at runtime, the user must supply the memory that the heap will manage. It is up to the caller to align the buffer as needed.
This parameter is ignored when creating heaps during configuration.
The documentation for this struct was generated from the following file: