SYS/BIOS
7.00
|
#include <ti/sysbios/heaps/HeapMem.h>
Data Fields | |
size_t | minBlockAlign |
Minimum alignment for each block allocated. More... | |
void * | buf |
Buffer being managed by this heap instance. More... | |
size_t | size |
Size of buffer being managed by this heap instance. More... | |
size_t HeapMem_Params::minBlockAlign |
Minimum alignment for each block allocated.
This parameter dictates the minimum alignment for each block that is allocated. If an alignment request of greater than minBlockAlign is made in the alloc, it will be honored. If an alignment request of less than minBlockAlign is made, the request will be ignored and minBlockAlign will be used.
The default alignment is 0 (which means this parameter is ignored).
void* HeapMem_Params::buf |
Buffer being managed by this heap instance.
This parameter is ignored in the static HeapMem.create() call. It is a required parameter in the dynamic HeapMem_create() call.
HeapMem requires that the buffer be aligned on a target-specific minimum alignment, and will adjust the buffer's start address and size as necessary to satisfy this requirement.
size_t HeapMem_Params::size |
Size of buffer being managed by this heap instance.
The usable size may be smaller depending on alignment requirements.