SYS/BIOS  7.00
Data Fields
Task_Stat Struct Reference

#include <ti/sysbios/knl/Task.h>

Data Fields

int priority
 Task priority. More...
 
void * stack
 Task stack pointer. Default = null. More...
 
size_t stackSize
 Task stack size. More...
 
IHeap_Handle stackHeap
 Mem heap used for dynamically created task stack. More...
 
void * env
 Global environment struct. More...
 
Task_Mode mode
 
void * sp
 Task's current stack pointer. More...
 
size_t used
 

Field Documentation

§ priority

int Task_Stat::priority

Task priority.

§ stack

void* Task_Stat::stack

Task stack pointer. Default = null.

Null indicates that the stack is to be allocated by create().

§ stackSize

size_t Task_Stat::stackSize

Task stack size.

§ stackHeap

IHeap_Handle Task_Stat::stackHeap

Mem heap used for dynamically created task stack.

The default value of NULL means that BIOS heap is used.

§ env

void* Task_Stat::env

Global environment struct.

§ mode

Task_Mode Task_Stat::mode

§ sp

void* Task_Stat::sp

Task's current stack pointer.

§ used

size_t Task_Stat::used

The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale