TI-15.4 Stack API
5.30.00.26
|
#include <api_mac.h>
Data Fields | |
ApiMac_sec_t | sec |
ApiMac_sAddrExt_t | orphanAddress |
uint16_t | shortAddress |
bool | associatedMember |
MLME orphan response type
ApiMac_sec_t _apimac_mlmeorphanrsp::sec |
The security parameters for this message
ApiMac_sAddrExt_t _apimac_mlmeorphanrsp::orphanAddress |
The extended address of the device sending the orphan notification
uint16_t _apimac_mlmeorphanrsp::shortAddress |
The short address of the orphaned device
bool _apimac_mlmeorphanrsp::associatedMember |
TRUE if the orphaned device is associated with this coordinator