![]() |
![]() |
TI-15.4 Stack API
5.30.00.26
|
#include <api_mac.h>
Data Fields | |
ApiMac_sec_t | sec |
uint8_t | logicalChannel |
uint8_t | channelPage |
uint8_t | phyID |
ApiMac_sAddr_t | coordAddress |
uint16_t | coordPanId |
ApiMac_capabilityInfo_t | capabilityInformation |
MLME associate request type
ApiMac_sec_t _apimac_macmlmeassociatereq::sec |
The security parameters for this message
uint8_t _apimac_macmlmeassociatereq::logicalChannel |
The channel on which to attempt association
uint8_t _apimac_macmlmeassociatereq::channelPage |
The channel page on which to attempt association
uint8_t _apimac_macmlmeassociatereq::phyID |
Identifier for the PHY descriptor
ApiMac_sAddr_t _apimac_macmlmeassociatereq::coordAddress |
Address of the coordinator with which to associate
uint16_t _apimac_macmlmeassociatereq::coordPanId |
The identifier of the PAN with which to associate
ApiMac_capabilityInfo_t _apimac_macmlmeassociatereq::capabilityInformation |
The operational capabilities of this device