![]() |
![]() |
rflib
|
IEEE 802.15.4 Receive Command. More...
#include <rf_ieee_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x2801. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More... | |
} | condition |
uint8_t | channel |
Channel to tune to in the start of the operation 0: Use existing channel 11–26: Use as IEEE 802.15.4 channel, i.e. frequency is (2405 + 5 × (channel - 11)) MHz 60–207: Frequency is (2300 + channel) MHz Others: Reserved More... | |
struct { | |
uint8_t bAutoFlushCrc:1 | |
If 1, automatically remove packets with CRC error from Rx queue. More... | |
uint8_t bAutoFlushIgn:1 | |
If 1, automatically remove packets that can be ignored according to frame filtering from Rx queue. More... | |
uint8_t bIncludePhyHdr:1 | |
If 1, include the received PHY header field in the stored packet; otherwise discard it. More... | |
uint8_t bIncludeCrc:1 | |
If 1, include the received CRC field in the stored packet; otherwise discard it. More... | |
uint8_t bAppendRssi:1 | |
If 1, append an RSSI byte to the packet in the Rx queue. More... | |
uint8_t bAppendCorrCrc:1 | |
If 1, append a correlation value and CRC result byte to the packet in the Rx queue. More... | |
uint8_t bAppendSrcInd:1 | |
If 1, append an index from the source matching algorithm. More... | |
uint8_t bAppendTimestamp:1 | |
If 1, append a timestamp to the packet in the Rx queue. More... | |
} | rxConfig |
dataQueue_t * | pRxQ |
Pointer to receive queue. More... | |
rfc_ieeeRxOutput_t * | pOutput |
Pointer to output structure (NULL: Do not store results) More... | |
struct { | |
uint16_t frameFiltEn:1 | |
0: Disable frame filtering 1: Enable frame filtering More... | |
uint16_t frameFiltStop:1 | |
0: Receive all packets to the end 1: Stop receiving frame once frame filtering has caused the frame to be rejected. More... | |
uint16_t autoAckEn:1 | |
0: Disable auto ACK 1: Enable auto ACK. More... | |
uint16_t slottedAckEn:1 | |
0: Non-slotted ACK 1: Slotted ACK. More... | |
uint16_t autoPendEn:1 | |
0: Auto-pend disabled 1: Auto-pend enabled More... | |
uint16_t defaultPend:1 | |
The value of the pending data bit in auto ACK packets that are not subject to auto-pend. More... | |
uint16_t bPendDataReqOnly:1 | |
0: Use auto-pend for any packet 1: Use auto-pend for data request packets only More... | |
uint16_t bPanCoord:1 | |
0: Device is not PAN coordinator 1: Device is PAN coordinator More... | |
uint16_t maxFrameVersion:2 | |
Reject frames where the frame version field in the FCF is greater than this value. More... | |
uint16_t fcfReservedMask:3 | |
Value to be AND-ed with the reserved part of the FCF; frame rejected if result is non-zero. More... | |
uint16_t modifyFtFilter:2 | |
Treatment of MSB of frame type field before frame-type filtering: 0: No modification 1: Invert MSB 2: Set MSB to 0 3: Set MSB to 1. More... | |
uint16_t bStrictLenFilter:1 | |
0: Accept acknowledgement frames of any length >= 5 1: Accept only acknowledgement frames of length 5 More... | |
} | frameFiltOpt |
Frame filtering options. More... | |
struct { | |
uint8_t bAcceptFt0Beacon:1 | |
Treatment of frames with frame type 000 (beacon): 0: Reject 1: Accept. More... | |
uint8_t bAcceptFt1Data:1 | |
Treatment of frames with frame type 001 (data): 0: Reject 1: Accept. More... | |
uint8_t bAcceptFt2Ack:1 | |
Treatment of frames with frame type 010 (ACK): 0: Reject, unless running ACK receive command 1: Always accept. More... | |
uint8_t bAcceptFt3MacCmd:1 | |
Treatment of frames with frame type 011 (MAC command): 0: Reject 1: Accept. More... | |
uint8_t bAcceptFt4Reserved:1 | |
Treatment of frames with frame type 100 (reserved): 0: Reject 1: Accept. More... | |
uint8_t bAcceptFt5Reserved:1 | |
Treatment of frames with frame type 101 (reserved): 0: Reject 1: Accept. More... | |
uint8_t bAcceptFt6Reserved:1 | |
Treatment of frames with frame type 110 (reserved): 0: Reject 1: Accept. More... | |
uint8_t bAcceptFt7Reserved:1 | |
Treatment of frames with frame type 111 (reserved): 0: Reject 1: Accept. More... | |
} | frameTypes |
Frame types to receive in frame filtering. More... | |
struct { | |
uint8_t ccaEnEnergy:1 | |
Enable energy scan as CCA source. More... | |
uint8_t ccaEnCorr:1 | |
Enable correlator based carrier sense as CCA source. More... | |
uint8_t ccaEnSync:1 | |
Enable sync found based carrier sense as CCA source. More... | |
uint8_t ccaCorrOp:1 | |
Operator to use between energy based and correlator based CCA 0: Report busy channel if either ccaEnergy or ccaCorr are busy 1: Report busy channel if both ccaEnergy and ccaCorr are busy. More... | |
uint8_t ccaSyncOp:1 | |
Operator to use between sync found based CCA and the others 0: Always report busy channel if ccaSync is busy 1: Always report idle channel if ccaSync is idle. More... | |
uint8_t ccaCorrThr:2 | |
Threshold for number of correlation peaks in correlator based carrier sense. More... | |
} | ccaOpt |
CCA options. More... | |
int8_t | ccaRssiThr |
RSSI threshold for CCA. More... | |
uint8_t | __dummy0 |
uint8_t | numExtEntries |
Number of extended address entries. More... | |
uint8_t | numShortEntries |
Number of short address entries. More... | |
uint32_t * | pExtEntryList |
Pointer to list of extended address entries. More... | |
uint32_t * | pShortEntryList |
Pointer to list of short address entries. More... | |
uint64_t | localExtAddr |
The extended address of the local device. More... | |
uint16_t | localShortAddr |
The short address of the local device. More... | |
uint16_t | localPanID |
The PAN ID of the local device. More... | |
uint16_t | __dummy1 |
uint8_t | __dummy2 |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | endTrigger |
Trigger that causes the device to end the Rx operation. More... | |
ratmr_t | endTime |
Time used together with endTrigger that causes the device to end the Rx operation. More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More... | |
} | condition |
struct { | |
uint8_t bAutoFlushCrc:1 | |
If 1, automatically remove packets with CRC error from Rx queue. More... | |
uint8_t bAutoFlushIgn:1 | |
If 1, automatically remove packets that can be ignored according to frame filtering from Rx queue. More... | |
uint8_t bIncludePhyHdr:1 | |
If 1, include the received PHY header field in the stored packet; otherwise discard it. More... | |
uint8_t bIncludeCrc:1 | |
If 1, include the received CRC field in the stored packet; otherwise discard it. More... | |
uint8_t bAppendRssi:1 | |
If 1, append an RSSI byte to the packet in the Rx queue. More... | |
uint8_t bAppendCorrCrc:1 | |
If 1, append a correlation value and CRC result byte to the packet in the Rx queue. More... | |
uint8_t bAppendSrcInd:1 | |
If 1, append an index from the source matching algorithm. More... | |
uint8_t bAppendTimestamp:1 | |
If 1, append a timestamp to the packet in the Rx queue. More... | |
} | rxConfig |
struct { | |
uint16_t frameFiltEn:1 | |
0: Disable frame filtering 1: Enable frame filtering More... | |
uint16_t frameFiltStop:1 | |
0: Receive all packets to the end 1: Stop receiving frame once frame filtering has caused the frame to be rejected. More... | |
uint16_t autoAckEn:1 | |
0: Disable auto ACK 1: Enable auto ACK. More... | |
uint16_t slottedAckEn:1 | |
0: Non-slotted ACK 1: Slotted ACK. More... | |
uint16_t autoPendEn:1 | |
0: Auto-pend disabled 1: Auto-pend enabled More... | |
uint16_t defaultPend:1 | |
The value of the pending data bit in auto ACK packets that are not subject to auto-pend. More... | |
uint16_t bPendDataReqOnly:1 | |
0: Use auto-pend for any packet 1: Use auto-pend for data request packets only More... | |
uint16_t bPanCoord:1 | |
0: Device is not PAN coordinator 1: Device is PAN coordinator More... | |
uint16_t maxFrameVersion:2 | |
Reject frames where the frame version field in the FCF is greater than this value. More... | |
uint16_t fcfReservedMask:3 | |
Value to be AND-ed with the reserved part of the FCF; frame rejected if result is non-zero. More... | |
uint16_t modifyFtFilter:2 | |
Treatment of MSB of frame type field before frame-type filtering: 0: No modification 1: Invert MSB 2: Set MSB to 0 3: Set MSB to 1. More... | |
uint16_t bStrictLenFilter:1 | |
0: Accept acknowledgement frames of any length >= 5 1: Accept only acknowledgement frames of length 5 More... | |
} | frameFiltOpt |
Frame filtering options. More... | |
struct { | |
uint8_t bAcceptFt0Beacon:1 | |
Treatment of frames with frame type 000 (beacon): 0: Reject 1: Accept. More... | |
uint8_t bAcceptFt1Data:1 | |
Treatment of frames with frame type 001 (data): 0: Reject 1: Accept. More... | |
uint8_t bAcceptFt2Ack:1 | |
Treatment of frames with frame type 010 (ACK): 0: Reject, unless running ACK receive command 1: Always accept. More... | |
uint8_t bAcceptFt3MacCmd:1 | |
Treatment of frames with frame type 011 (MAC command): 0: Reject 1: Accept. More... | |
uint8_t bAcceptFt4Reserved:1 | |
Treatment of frames with frame type 100 (reserved): 0: Reject 1: Accept. More... | |
uint8_t bAcceptFt5Reserved:1 | |
Treatment of frames with frame type 101 (reserved): 0: Reject 1: Accept. More... | |
uint8_t bAcceptFt6Reserved:1 | |
Treatment of frames with frame type 110 (reserved): 0: Reject 1: Accept. More... | |
uint8_t bAcceptFt7Reserved:1 | |
Treatment of frames with frame type 111 (reserved): 0: Reject 1: Accept. More... | |
} | frameTypes |
Frame types to receive in frame filtering. More... | |
struct { | |
uint8_t ccaEnEnergy:1 | |
Enable energy scan as CCA source. More... | |
uint8_t ccaEnCorr:1 | |
Enable correlator based carrier sense as CCA source. More... | |
uint8_t ccaEnSync:1 | |
Enable sync found based carrier sense as CCA source. More... | |
uint8_t ccaCorrOp:1 | |
Operator to use between energy based and correlator based CCA 0: Report busy channel if either ccaEnergy or ccaCorr are busy 1: Report busy channel if both ccaEnergy and ccaCorr are busy. More... | |
uint8_t ccaSyncOp:1 | |
Operator to use between sync found based CCA and the others 0: Always report busy channel if ccaSync is busy 1: Always report idle channel if ccaSync is idle. More... | |
uint8_t ccaCorrThr:2 | |
Threshold for number of correlation peaks in correlator based carrier sense. More... | |
} | ccaOpt |
CCA options. More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | endTrigger |
Trigger that causes the device to end the Rx operation. More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More... | |
} | condition |
struct { | |
uint8_t bAutoFlushCrc:1 | |
If 1, automatically remove packets with CRC error from Rx queue. More... | |
uint8_t bAutoFlushIgn:1 | |
If 1, automatically remove packets that can be ignored according to frame filtering from Rx queue. More... | |
uint8_t bIncludePhyHdr:1 | |
If 1, include the received PHY header field in the stored packet; otherwise discard it. More... | |
uint8_t bIncludeCrc:1 | |
If 1, include the received CRC field in the stored packet; otherwise discard it. More... | |
uint8_t bAppendRssi:1 | |
If 1, append an RSSI byte to the packet in the Rx queue. More... | |
uint8_t bAppendCorrCrc:1 | |
If 1, append a correlation value and CRC result byte to the packet in the Rx queue. More... | |
uint8_t bAppendSrcInd:1 | |
If 1, append an index from the source matching algorithm. More... | |
uint8_t bAppendTimestamp:1 | |
If 1, append a timestamp to the packet in the Rx queue. More... | |
} | rxConfig |
struct { | |
uint16_t frameFiltEn:1 | |
0: Disable frame filtering 1: Enable frame filtering More... | |
uint16_t frameFiltStop:1 | |
0: Receive all packets to the end 1: Stop receiving frame once frame filtering has caused the frame to be rejected. More... | |
uint16_t autoAckEn:1 | |
0: Disable auto ACK 1: Enable auto ACK. More... | |
uint16_t slottedAckEn:1 | |
0: Non-slotted ACK 1: Slotted ACK. More... | |
uint16_t autoPendEn:1 | |
0: Auto-pend disabled 1: Auto-pend enabled More... | |
uint16_t defaultPend:1 | |
The value of the pending data bit in auto ACK packets that are not subject to auto-pend. More... | |
uint16_t bPendDataReqOnly:1 | |
0: Use auto-pend for any packet 1: Use auto-pend for data request packets only More... | |
uint16_t bPanCoord:1 | |
0: Device is not PAN coordinator 1: Device is PAN coordinator More... | |
uint16_t maxFrameVersion:2 | |
Reject frames where the frame version field in the FCF is greater than this value. More... | |
uint16_t fcfReservedMask:3 | |
Value to be AND-ed with the reserved part of the FCF; frame rejected if result is non-zero. More... | |
uint16_t modifyFtFilter:2 | |
Treatment of MSB of frame type field before frame-type filtering: 0: No modification 1: Invert MSB 2: Set MSB to 0 3: Set MSB to 1. More... | |
uint16_t bStrictLenFilter:1 | |
0: Accept acknowledgement frames of any length >= 5 1: Accept only acknowledgement frames of length 5 More... | |
} | frameFiltOpt |
Frame filtering options. More... | |
struct { | |
uint8_t bAcceptFt0Beacon:1 | |
Treatment of frames with frame type 000 (beacon): 0: Reject 1: Accept. More... | |
uint8_t bAcceptFt1Data:1 | |
Treatment of frames with frame type 001 (data): 0: Reject 1: Accept. More... | |
uint8_t bAcceptFt2Ack:1 | |
Treatment of frames with frame type 010 (ACK): 0: Reject, unless running ACK receive command 1: Always accept. More... | |
uint8_t bAcceptFt3MacCmd:1 | |
Treatment of frames with frame type 011 (MAC command): 0: Reject 1: Accept. More... | |
uint8_t bAcceptFt4Reserved:1 | |
Treatment of frames with frame type 100 (reserved): 0: Reject 1: Accept. More... | |
uint8_t bAcceptFt5Reserved:1 | |
Treatment of frames with frame type 101 (reserved): 0: Reject 1: Accept. More... | |
uint8_t bAcceptFt6Reserved:1 | |
Treatment of frames with frame type 110 (reserved): 0: Reject 1: Accept. More... | |
uint8_t bAcceptFt7Reserved:1 | |
Treatment of frames with frame type 111 (reserved): 0: Reject 1: Accept. More... | |
} | frameTypes |
Frame types to receive in frame filtering. More... | |
struct { | |
uint8_t ccaEnEnergy:1 | |
Enable energy scan as CCA source. More... | |
uint8_t ccaEnCorr:1 | |
Enable correlator based carrier sense as CCA source. More... | |
uint8_t ccaEnSync:1 | |
Enable sync found based carrier sense as CCA source. More... | |
uint8_t ccaCorrOp:1 | |
Operator to use between energy based and correlator based CCA 0: Report busy channel if either ccaEnergy or ccaCorr are busy 1: Report busy channel if both ccaEnergy and ccaCorr are busy. More... | |
uint8_t ccaSyncOp:1 | |
Operator to use between sync found based CCA and the others 0: Always report busy channel if ccaSync is busy 1: Always report idle channel if ccaSync is idle. More... | |
uint8_t ccaCorrThr:2 | |
Threshold for number of correlation peaks in correlator based carrier sense. More... | |
} | ccaOpt |
CCA options. More... | |
uint8_t | dualPanEn |
Dual PAN support 0: Single PAN; legacy command structure supported 1: Dual PAN enabled. More... | |
uint16_t | __dummy0 |
uint8_t | __dummy1 |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | endTrigger |
Trigger that causes the device to end the Rx operation. More... | |
struct { | |
uint16_t frameFilterDoneEn0:1 | |
0: Disable frame filtering done interrupt on PAN 0 1: Enable frame filtering done interrupt on PAN 0. More... | |
uint16_t frameFilterDoneEn1:1 | |
0: Disable frame filtering done interrupt on PAN 1 1: Enable frame filtering done interrupt on PAN 1. More... | |
uint16_t autoAckEn0:1 | |
0: Disable auto ACK on PAN 0 1: Enable auto ACK on PAN 0. More... | |
uint16_t autoAckEn1:1 | |
0: Disable auto ACK on PAN 1 1: Enable auto ACK on PAN 1. More... | |
uint16_t autoPendEn0:1 | |
0: Auto-pend disabled on PAN 0 1: Auto-pend enabled on PAN 0 More... | |
uint16_t autoPendEn1:1 | |
0: Auto-pend disabled on PAN 1 1: Auto-pend enabled on PAN 1 More... | |
uint16_t bPendDataReqOnly0:1 | |
0: Use auto-pend for any packet on PAN 0 1: Use auto-pend for data request packets only on PAN 0 More... | |
uint16_t bPendDataReqOnly1:1 | |
0: Use auto-pend for any packet on PAN 1 1: Use auto-pend for data request packets only on PAN 1 More... | |
uint16_t bPanCoord0:1 | |
0: Device on PAN 0 is not PAN coordinator 1: Device on PAN 0 is PAN coordinator More... | |
uint16_t bPanCoord1:1 | |
0: Device on PAN 1 is not PAN coordinator 1: Device on PAN 1 is PAN coordinator More... | |
uint16_t bAllowEnhAck0:1 | |
0: Do not accept Enh-Ack on PAN 0 1: Accept Enh-Ack on PAN 0 More... | |
uint16_t bAllowEnhAck1:1 | |
0: Do not accept Enh-Ack on PAN 1 1: Accept Enh-Ack on PAN 1 More... | |
} | dualPanFiltOpt |
Dual PAN frame filtering options. More... | |
uint8_t | numExtEntries1 |
Number of extended address entries for PAN 1. More... | |
uint8_t | numShortEntries1 |
Number of short address entries for PAN 1. More... | |
uint32_t * | pExtEntryList1 |
Pointer to list of extended address entries for PAN 1. More... | |
uint32_t * | pShortEntryList1 |
Pointer to list of short address entries for PAN 1. More... | |
uint64_t | localExtAddr1 |
The extended address of the local device on PAN 1. More... | |
uint16_t | localShortAddr1 |
The short address of the local device on PAN 1. More... | |
uint16_t | localPanID1 |
The PAN ID of the local device on PAN 1. More... | |
IEEE 802.15.4 Receive Command.
uint16_t rfc_CMD_IEEE_RX_s::commandNo |
The command ID number 0x2801.
uint16_t rfc_CMD_IEEE_RX_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
rfc_radioOp_t * rfc_CMD_IEEE_RX_s::pNextOp |
Pointer to the next operation to run after this operation is done.
ratmr_t rfc_CMD_IEEE_RX_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
uint8_t rfc_CMD_IEEE_RX_s::triggerType |
The type of trigger.
uint8_t rfc_CMD_IEEE_RX_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
uint8_t rfc_CMD_IEEE_RX_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
uint8_t rfc_CMD_IEEE_RX_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
struct { ... } rfc_CMD_IEEE_RX_s::startTrigger |
Identification of the trigger that starts the operation.
uint8_t rfc_CMD_IEEE_RX_s::rule |
Condition for running next command: Rule for how to proceed.
uint8_t rfc_CMD_IEEE_RX_s::nSkip |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...
struct { ... } rfc_CMD_IEEE_RX_s::condition |
uint8_t rfc_CMD_IEEE_RX_s::channel |
Channel to tune to in the start of the operation
0: Use existing channel
11–26: Use as IEEE 802.15.4 channel, i.e. frequency is (2405 + 5 × (channel - 11)) MHz
60–207: Frequency is (2300 + channel) MHz
Others: Reserved
uint8_t rfc_CMD_IEEE_RX_s::bAutoFlushCrc |
If 1, automatically remove packets with CRC error from Rx queue.
uint8_t rfc_CMD_IEEE_RX_s::bAutoFlushIgn |
If 1, automatically remove packets that can be ignored according to frame filtering from Rx queue.
uint8_t rfc_CMD_IEEE_RX_s::bIncludePhyHdr |
If 1, include the received PHY header field in the stored packet; otherwise discard it.
uint8_t rfc_CMD_IEEE_RX_s::bIncludeCrc |
If 1, include the received CRC field in the stored packet; otherwise discard it.
uint8_t rfc_CMD_IEEE_RX_s::bAppendRssi |
If 1, append an RSSI byte to the packet in the Rx queue.
uint8_t rfc_CMD_IEEE_RX_s::bAppendCorrCrc |
If 1, append a correlation value and CRC result byte to the packet in the Rx queue.
uint8_t rfc_CMD_IEEE_RX_s::bAppendSrcInd |
If 1, append an index from the source matching algorithm.
uint8_t rfc_CMD_IEEE_RX_s::bAppendTimestamp |
If 1, append a timestamp to the packet in the Rx queue.
struct { ... } rfc_CMD_IEEE_RX_s::rxConfig |
dataQueue_t * rfc_CMD_IEEE_RX_s::pRxQ |
Pointer to receive queue.
rfc_ieeeRxOutput_t * rfc_CMD_IEEE_RX_s::pOutput |
Pointer to output structure (NULL: Do not store results)
uint16_t rfc_CMD_IEEE_RX_s::frameFiltEn |
0: Disable frame filtering
1: Enable frame filtering
uint16_t rfc_CMD_IEEE_RX_s::frameFiltStop |
0: Receive all packets to the end
1: Stop receiving frame once frame filtering has caused the frame to be rejected.
uint16_t rfc_CMD_IEEE_RX_s::autoAckEn |
0: Disable auto ACK
1: Enable auto ACK.
uint16_t rfc_CMD_IEEE_RX_s::slottedAckEn |
0: Non-slotted ACK
1: Slotted ACK.
uint16_t rfc_CMD_IEEE_RX_s::autoPendEn |
0: Auto-pend disabled
1: Auto-pend enabled
uint16_t rfc_CMD_IEEE_RX_s::defaultPend |
The value of the pending data bit in auto ACK packets that are not subject to auto-pend.
uint16_t rfc_CMD_IEEE_RX_s::bPendDataReqOnly |
0: Use auto-pend for any packet
1: Use auto-pend for data request packets only
uint16_t rfc_CMD_IEEE_RX_s::bPanCoord |
0: Device is not PAN coordinator
1: Device is PAN coordinator
uint16_t rfc_CMD_IEEE_RX_s::maxFrameVersion |
Reject frames where the frame version field in the FCF is greater than this value.
uint16_t rfc_CMD_IEEE_RX_s::fcfReservedMask |
Value to be AND-ed with the reserved part of the FCF; frame rejected if result is non-zero.
uint16_t rfc_CMD_IEEE_RX_s::modifyFtFilter |
Treatment of MSB of frame type field before frame-type filtering:
0: No modification
1: Invert MSB
2: Set MSB to 0
3: Set MSB to 1.
uint16_t rfc_CMD_IEEE_RX_s::bStrictLenFilter |
0: Accept acknowledgement frames of any length >= 5
1: Accept only acknowledgement frames of length 5
struct { ... } rfc_CMD_IEEE_RX_s::frameFiltOpt |
Frame filtering options.
uint8_t rfc_CMD_IEEE_RX_s::bAcceptFt0Beacon |
Treatment of frames with frame type 000 (beacon):
0: Reject
1: Accept.
uint8_t rfc_CMD_IEEE_RX_s::bAcceptFt1Data |
Treatment of frames with frame type 001 (data):
0: Reject
1: Accept.
uint8_t rfc_CMD_IEEE_RX_s::bAcceptFt2Ack |
Treatment of frames with frame type 010 (ACK):
0: Reject, unless running ACK receive command
1: Always accept.
uint8_t rfc_CMD_IEEE_RX_s::bAcceptFt3MacCmd |
Treatment of frames with frame type 011 (MAC command):
0: Reject
1: Accept.
uint8_t rfc_CMD_IEEE_RX_s::bAcceptFt4Reserved |
Treatment of frames with frame type 100 (reserved):
0: Reject
1: Accept.
uint8_t rfc_CMD_IEEE_RX_s::bAcceptFt5Reserved |
Treatment of frames with frame type 101 (reserved):
0: Reject
1: Accept.
uint8_t rfc_CMD_IEEE_RX_s::bAcceptFt6Reserved |
Treatment of frames with frame type 110 (reserved):
0: Reject
1: Accept.
uint8_t rfc_CMD_IEEE_RX_s::bAcceptFt7Reserved |
Treatment of frames with frame type 111 (reserved):
0: Reject
1: Accept.
struct { ... } rfc_CMD_IEEE_RX_s::frameTypes |
Frame types to receive in frame filtering.
uint8_t rfc_CMD_IEEE_RX_s::ccaEnEnergy |
Enable energy scan as CCA source.
uint8_t rfc_CMD_IEEE_RX_s::ccaEnCorr |
Enable correlator based carrier sense as CCA source.
uint8_t rfc_CMD_IEEE_RX_s::ccaEnSync |
Enable sync found based carrier sense as CCA source.
uint8_t rfc_CMD_IEEE_RX_s::ccaCorrOp |
Operator to use between energy based and correlator based CCA
0: Report busy channel if either ccaEnergy or ccaCorr are busy
1: Report busy channel if both ccaEnergy and ccaCorr are busy.
uint8_t rfc_CMD_IEEE_RX_s::ccaSyncOp |
Operator to use between sync found based CCA and the others
0: Always report busy channel if ccaSync is busy
1: Always report idle channel if ccaSync is idle.
uint8_t rfc_CMD_IEEE_RX_s::ccaCorrThr |
Threshold for number of correlation peaks in correlator based carrier sense.
struct { ... } rfc_CMD_IEEE_RX_s::ccaOpt |
CCA options.
int8_t rfc_CMD_IEEE_RX_s::ccaRssiThr |
RSSI threshold for CCA.
uint8_t rfc_CMD_IEEE_RX_s::__dummy0 |
uint8_t rfc_CMD_IEEE_RX_s::numExtEntries |
Number of extended address entries.
uint8_t rfc_CMD_IEEE_RX_s::numShortEntries |
Number of short address entries.
uint32_t * rfc_CMD_IEEE_RX_s::pExtEntryList |
Pointer to list of extended address entries.
uint32_t * rfc_CMD_IEEE_RX_s::pShortEntryList |
Pointer to list of short address entries.
uint64_t rfc_CMD_IEEE_RX_s::localExtAddr |
The extended address of the local device.
uint16_t rfc_CMD_IEEE_RX_s::localShortAddr |
The short address of the local device.
uint16_t rfc_CMD_IEEE_RX_s::localPanID |
The PAN ID of the local device.
uint16_t rfc_CMD_IEEE_RX_s::__dummy1 |
uint8_t rfc_CMD_IEEE_RX_s::__dummy2 |
struct { ... } rfc_CMD_IEEE_RX_s::endTrigger |
Trigger that causes the device to end the Rx operation.
ratmr_t rfc_CMD_IEEE_RX_s::endTime |
Time used together with endTrigger
that causes the device to end the Rx operation.
struct { ... } rfc_CMD_IEEE_RX_s::startTrigger |
Identification of the trigger that starts the operation.
struct { ... } rfc_CMD_IEEE_RX_s::condition |
struct { ... } rfc_CMD_IEEE_RX_s::rxConfig |
struct { ... } rfc_CMD_IEEE_RX_s::frameFiltOpt |
Frame filtering options.
struct { ... } rfc_CMD_IEEE_RX_s::frameTypes |
Frame types to receive in frame filtering.
struct { ... } rfc_CMD_IEEE_RX_s::ccaOpt |
CCA options.
struct { ... } rfc_CMD_IEEE_RX_s::endTrigger |
Trigger that causes the device to end the Rx operation.
struct { ... } rfc_CMD_IEEE_RX_s::startTrigger |
Identification of the trigger that starts the operation.
struct { ... } rfc_CMD_IEEE_RX_s::condition |
struct { ... } rfc_CMD_IEEE_RX_s::rxConfig |
struct { ... } rfc_CMD_IEEE_RX_s::frameFiltOpt |
Frame filtering options.
struct { ... } rfc_CMD_IEEE_RX_s::frameTypes |
Frame types to receive in frame filtering.
struct { ... } rfc_CMD_IEEE_RX_s::ccaOpt |
CCA options.
uint8_t rfc_CMD_IEEE_RX_s::dualPanEn |
Dual PAN support
0: Single PAN; legacy command structure supported
1: Dual PAN enabled.
uint16_t rfc_CMD_IEEE_RX_s::__dummy0 |
uint8_t rfc_CMD_IEEE_RX_s::__dummy1 |
struct { ... } rfc_CMD_IEEE_RX_s::endTrigger |
Trigger that causes the device to end the Rx operation.
uint16_t rfc_CMD_IEEE_RX_s::frameFilterDoneEn0 |
0: Disable frame filtering done interrupt on PAN 0
1: Enable frame filtering done interrupt on PAN 0.
uint16_t rfc_CMD_IEEE_RX_s::frameFilterDoneEn1 |
0: Disable frame filtering done interrupt on PAN 1
1: Enable frame filtering done interrupt on PAN 1.
uint16_t rfc_CMD_IEEE_RX_s::autoAckEn0 |
0: Disable auto ACK on PAN 0
1: Enable auto ACK on PAN 0.
uint16_t rfc_CMD_IEEE_RX_s::autoAckEn1 |
0: Disable auto ACK on PAN 1
1: Enable auto ACK on PAN 1.
uint16_t rfc_CMD_IEEE_RX_s::autoPendEn0 |
0: Auto-pend disabled on PAN 0
1: Auto-pend enabled on PAN 0
uint16_t rfc_CMD_IEEE_RX_s::autoPendEn1 |
0: Auto-pend disabled on PAN 1
1: Auto-pend enabled on PAN 1
uint16_t rfc_CMD_IEEE_RX_s::bPendDataReqOnly0 |
0: Use auto-pend for any packet on PAN 0
1: Use auto-pend for data request packets only on PAN 0
uint16_t rfc_CMD_IEEE_RX_s::bPendDataReqOnly1 |
0: Use auto-pend for any packet on PAN 1
1: Use auto-pend for data request packets only on PAN 1
uint16_t rfc_CMD_IEEE_RX_s::bPanCoord0 |
0: Device on PAN 0 is not PAN coordinator
1: Device on PAN 0 is PAN coordinator
uint16_t rfc_CMD_IEEE_RX_s::bPanCoord1 |
0: Device on PAN 1 is not PAN coordinator
1: Device on PAN 1 is PAN coordinator
uint16_t rfc_CMD_IEEE_RX_s::bAllowEnhAck0 |
0: Do not accept Enh-Ack on PAN 0
1: Accept Enh-Ack on PAN 0
uint16_t rfc_CMD_IEEE_RX_s::bAllowEnhAck1 |
0: Do not accept Enh-Ack on PAN 1
1: Accept Enh-Ack on PAN 1
struct { ... } rfc_CMD_IEEE_RX_s::dualPanFiltOpt |
Dual PAN frame filtering options.
uint8_t rfc_CMD_IEEE_RX_s::numExtEntries1 |
Number of extended address entries for PAN 1.
uint8_t rfc_CMD_IEEE_RX_s::numShortEntries1 |
Number of short address entries for PAN 1.
uint32_t* rfc_CMD_IEEE_RX_s::pExtEntryList1 |
Pointer to list of extended address entries for PAN 1.
uint32_t* rfc_CMD_IEEE_RX_s::pShortEntryList1 |
Pointer to list of short address entries for PAN 1.
uint64_t rfc_CMD_IEEE_RX_s::localExtAddr1 |
The extended address of the local device on PAN 1.
uint16_t rfc_CMD_IEEE_RX_s::localShortAddr1 |
The short address of the local device on PAN 1.
uint16_t rfc_CMD_IEEE_RX_s::localPanID1 |
The PAN ID of the local device on PAN 1.