![]() |
![]() |
rflib
|
Set TX power with possibility to switch between PAs. More...
#include <rf_common_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x0015. More... | |
uint16_t | __dummy0 |
uint32_t * | pRegOverride |
Pointer to a list of hardware and configuration registers to override as part of the change, including new TX power. More... | |
Set TX power with possibility to switch between PAs.
uint16_t rfc_CMD_CHANGE_PA_s::commandNo |
The command ID number 0x0015.
uint16_t rfc_CMD_CHANGE_PA_s::__dummy0 |
uint32_t * rfc_CMD_CHANGE_PA_s::pRegOverride |
Pointer to a list of hardware and configuration registers to override as part of the change, including new TX power.