Data Fields
KeyStore_PreProvisionedKeyMetaData Struct Reference

Structure for storing pre-provisioned key's meta data. More...

#include <CryptoKeyKeyStore_PSA.h>

Data Fields

uint8_t header [(sizeof("HUK\EY"))]
 
uint32_t lifetime
 
KeyStore_PSA_KeyFileId id
 
uint32_t export
 
KeyStore_PSA_Algorithm alg
 
KeyStore_PSA_KeyUsage usage
 
uint32_t keyLength
 

Detailed Description

Structure for storing pre-provisioned key's meta data.

Field Documentation

§ header

uint8_t KeyStore_PreProvisionedKeyMetaData::header[(sizeof("HUK\KEY"))]

§ lifetime

uint32_t KeyStore_PreProvisionedKeyMetaData::lifetime

§ id

KeyStore_PSA_KeyFileId KeyStore_PreProvisionedKeyMetaData::id

§ export

uint32_t KeyStore_PreProvisionedKeyMetaData::export

§ alg

KeyStore_PSA_Algorithm KeyStore_PreProvisionedKeyMetaData::alg

§ usage

KeyStore_PSA_KeyUsage KeyStore_PreProvisionedKeyMetaData::usage

§ keyLength

uint32_t KeyStore_PreProvisionedKeyMetaData::keyLength

The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale