Data Fields
ECDSACC26X1_Object Struct Reference

ECDSACC26X1 Object. More...

#include <ECDSACC26X1.h>

Data Fields

bool isOpen
 
ECDSA_ReturnBehavior returnBehavior
 
ECC_State eccState
 
uint32_t eccWorkZone [288]
 

Detailed Description

ECDSACC26X1 Object.

The application must not access any member variables of this structure!

Field Documentation

§ isOpen

bool ECDSACC26X1_Object::isOpen

§ returnBehavior

ECDSA_ReturnBehavior ECDSACC26X1_Object::returnBehavior

§ eccState

ECC_State ECDSACC26X1_Object::eccState

§ eccWorkZone

uint32_t ECDSACC26X1_Object::eccWorkZone[288]

The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale