Data Fields
DACCC26XX_Object Struct Reference

DACCC26XX Object. More...

#include <DACCC26X2.h>

Data Fields

bool isEnabled
 
bool isOpen
 
uint32_t currCode
 
uint32_t dacOutputMin
 
uint32_t dacOutputMax
 

Detailed Description

DACCC26XX Object.

The application must not access any member variables of this structure!

Field Documentation

§ isEnabled

bool DACCC26XX_Object::isEnabled

< Flag to determine current state of the DAC's output Flag if the instance is in use

§ isOpen

bool DACCC26XX_Object::isOpen

Current DAC code set

§ currCode

uint32_t DACCC26XX_Object::currCode

Minimum DAC output in uV

§ dacOutputMin

uint32_t DACCC26XX_Object::dacOutputMin

Maximum DAC output in uV

§ dacOutputMax

uint32_t DACCC26XX_Object::dacOutputMax

The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale