Data Fields
AESCTRDRBG_Params Struct Reference

AESCTRDRBG Parameters. More...

#include <AESCTRDRBG.h>

Data Fields

AESCTRDRBG_AES_KEY_LENGTH keyLength
 
uint32_t reseedInterval
 
const void * seed
 
const void * personalizationData
 
size_t personalizationDataLength
 
AESCTRDRBG_ReturnBehavior returnBehavior
 
void * custom
 

Detailed Description

AESCTRDRBG Parameters.

AESCTRDRBG Parameters are used to with the AESCTRDRBG_open() call. Default values for these parameters are set using AESCTRDRBG_Params_init().

See also
AESCTRDRBG_Params_init()

Field Documentation

§ keyLength

AESCTRDRBG_AES_KEY_LENGTH AESCTRDRBG_Params::keyLength

Length of the internal AES key of the driver instance.

§ reseedInterval

uint32_t AESCTRDRBG_Params::reseedInterval

Number of random number generation requests before the application is required to reseed the driver.

§ seed

const void* AESCTRDRBG_Params::seed

Entropy used to seed the internal state of the driver. Must be one of AESCTRDRBG_SEED_LENGTH long depending on keyLength.

§ personalizationData

const void* AESCTRDRBG_Params::personalizationData

Optional non-secret personalization data to mix into the driver's internal state.

§ personalizationDataLength

size_t AESCTRDRBG_Params::personalizationDataLength

Length of the optional personalizationData. Must satisfy 0 <= personalizationDataLength <= seed length.

§ returnBehavior

AESCTRDRBG_ReturnBehavior AESCTRDRBG_Params::returnBehavior

Return behavior of the driver instance. AESCTRDRBG_RETURN_BEHAVIOR_POLLING is strongly recommended unless requests for > 500 bytes with AES-256 or 1250 bytes for AES-128 will be common use cases for this driver instance.

§ custom

void* AESCTRDRBG_Params::custom

Custom argument used by driver implementation


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale