Macros
Key policies

Macros

#define KEYSTORE_PSA_KEY_USAGE_EXPORT   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_EXPORT)
 
#define KEYSTORE_PSA_KEY_USAGE_COPY   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_COPY)
 
#define KEYSTORE_PSA_KEY_USAGE_ENCRYPT   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_ENCRYPT)
 
#define KEYSTORE_PSA_KEY_USAGE_DECRYPT   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_DECRYPT)
 
#define KEYSTORE_PSA_KEY_USAGE_SIGN_HASH   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_SIGN_HASH)
 
#define KEYSTORE_PSA_KEY_USAGE_VERIFY_HASH   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_VERIFY_HASH)
 
#define KEYSTORE_PSA_KEY_USAGE_DERIVE   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_DERIVE)
 

Detailed Description

Macro Definition Documentation

§ KEYSTORE_PSA_KEY_USAGE_EXPORT

#define KEYSTORE_PSA_KEY_USAGE_EXPORT   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_EXPORT)

Whether the key may be exported.

A public key or the public part of a key pair may always be exported regardless of the value of this permission flag.

If a key does not have export permission, implementations shall not allow the key to be exported in plain form from the cryptoprocessor, whether through KeyStore_PSA_exportKey() or through a proprietary interface. The key may however be exportable in a wrapped form, i.e. in a form where it is encrypted by another key.

§ KEYSTORE_PSA_KEY_USAGE_COPY

#define KEYSTORE_PSA_KEY_USAGE_COPY   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_COPY)

Whether the key may be copied.

This flag allows the use of KeyStore_PSA_copyKey() to make a copy of the key with the same policy or a more restrictive policy.

For lifetimes for which the key is located in a secure element which enforce the non-exportability of keys, copying a key outside the secure element also requires the usage flag KEYSTORE_PSA_KEY_USAGE_EXPORT. Copying the key inside the secure element is permitted with just KEYSTORE_PSA_KEY_USAGE_COPY if the secure element supports it. For keys with the lifetime KEYSTORE_PSA_KEY_LIFETIME_VOLATILE or KEYSTORE_PSA_KEY_LIFETIME_PERSISTENT, the usage flag KEYSTORE_PSA_KEY_USAGE_COPY is sufficient to permit the copy.

§ KEYSTORE_PSA_KEY_USAGE_ENCRYPT

#define KEYSTORE_PSA_KEY_USAGE_ENCRYPT   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_ENCRYPT)

Whether the key may be used to encrypt a message.

This flag allows the key to be used for a symmetric encryption operation, for an AEAD encryption-and-authentication operation, or for an asymmetric encryption operation, if otherwise permitted by the key's type and policy.

For a key pair, this concerns the public key.

§ KEYSTORE_PSA_KEY_USAGE_DECRYPT

#define KEYSTORE_PSA_KEY_USAGE_DECRYPT   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_DECRYPT)

Whether the key may be used to decrypt a message.

This flag allows the key to be used for a symmetric decryption operation, for an AEAD decryption-and-verification operation, or for an asymmetric decryption operation, if otherwise permitted by the key's type and policy.

For a key pair, this concerns the private key.

§ KEYSTORE_PSA_KEY_USAGE_SIGN_HASH

#define KEYSTORE_PSA_KEY_USAGE_SIGN_HASH   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_SIGN_HASH)

Whether the key may be used to sign a message.

This flag allows the key to be used for a MAC calculation operation or for an asymmetric signature operation, if otherwise permitted by the key's type and policy.

For a key pair, this concerns the private key.

§ KEYSTORE_PSA_KEY_USAGE_VERIFY_HASH

#define KEYSTORE_PSA_KEY_USAGE_VERIFY_HASH   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_VERIFY_HASH)

Whether the key may be used to verify a message signature.

This flag allows the key to be used for a MAC verification operation or for an asymmetric signature verification operation, if otherwise permitted by by the key's type and policy.

For a key pair, this concerns the public key.

§ KEYSTORE_PSA_KEY_USAGE_DERIVE

#define KEYSTORE_PSA_KEY_USAGE_DERIVE   ((KeyStore_PSA_KeyUsage)PSA_KEY_USAGE_DERIVE)

Whether the key may be used to derive other keys.

© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale