|
static uint32_t | TimerIntNumberGet (uint32_t ui32Base) |
| Gets the timer interrupt number. More...
|
|
void | TimerConfigure (uint32_t ui32Base, uint32_t ui32Config) |
| Configures the timer(s). More...
|
|
void | TimerLevelControl (uint32_t ui32Base, uint32_t ui32Timer, bool bInvert) |
| Controls the output level. More...
|
|
void | TimerStallControl (uint32_t ui32Base, uint32_t ui32Timer, bool bStall) |
| Controls the stall handling. More...
|
|
void | TimerWaitOnTriggerControl (uint32_t ui32Base, uint32_t ui32Timer, bool bWait) |
| Controls the wait on trigger handling. More...
|
|
void | TimerIntRegister (uint32_t ui32Base, uint32_t ui32Timer, void(*pfnHandler)(void)) |
| Registers an interrupt handler for the timer interrupt in the dynamic interrupt table. More...
|
|
void | TimerIntUnregister (uint32_t ui32Base, uint32_t ui32Timer) |
| Unregisters an interrupt handler for the timer interrupt in the dynamic interrupt table. More...
|
|
void | TimerMatchUpdateMode (uint32_t ui32Base, uint32_t ui32Timer, uint32_t ui32Mode) |
| Sets the Match Register Update mode. More...
|
|
void | TimerIntervalLoadMode (uint32_t ui32Base, uint32_t ui32Timer, uint32_t ui32Mode) |
| Sets the Interval Load mode. More...
|
|