TI BLE5-Stack API Documentation  2.02.07.00
Data Fields
rtlsSrv_clIQReport_t Struct Reference

CTE Connectionless IQ Report Event RTLSSRV_CL_CTE_IQ_REPORT_EVT. More...

Data Fields

uint8_t channelIndex
 index of data channel
 
uint8_t cteType
 cte type
 
uint16_t eventCounter
 periodic adv event counter
 
int8_t * iqSamples
 list of IQ samples, format is [i,q,i,q,i,q....]
 
uint8_t numAnt
 number of antennas we are using
 
uint8_t packetStatus
 packet status (success or CRC error)
 
uint16_t rssi
 current rssi
 
uint8_t rssiAntenna
 antenna ID
 
uint16_t sampleCount
 number of samples
 
uint8_t sampleCtrl
 default filtering or RAW_RF
 
uint8_t sampleRate
 sample rate of frontend: 1Mhz, 2Mhz, 3Mhz, 4Mhz
 
uint8_t sampleSize
 sample size: 8 or 16 bit samples
 
uint8_t slotDuration
 sampling slot 1us or 2us
 
uint16_t syncHandle
 sync handle
 

Detailed Description

CTE Connectionless IQ Report Event RTLSSRV_CL_CTE_IQ_REPORT_EVT.


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale