TI BLE5-Stack API Documentation  2.02.07.00
Data Fields
hciEvt_BLEPeriodicAdvSyncEstablished_t Struct Reference

LE Periodic Advertising Sync Established event. More...

Data Fields

uint8 address [B_ADDR_LEN]
 Peer address.
 
uint8 addrType
 Peer address type.
 
uint8 BLEEventCode
 BLE Event Code.
 
uint8 clockAccuracy
 Peer Clock Accuracy.
 
osal_event_hdr_t hdr
 osal event header
 
uint16 periodicInterval
 Periodic interval.
 
uint8 phy
 Peer PHY.
 
uint8 sid
 Peer SID.
 
uint8 status
 status of event
 
uint16 syncHandle
 sync handle
 

Detailed Description

LE Periodic Advertising Sync Established event.


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale