TI BLE5-Stack API Documentation  2.02.07.00
Data Fields
hciEvt_BLEPeriodicAdvReport_t Struct Reference

LE Periodic Advertising Report event. More...

Data Fields

uint8 BLEEventCode
 BLE Event Code.
 
uint8 cteType
 CTE type received.
 
uint8 * data
 Periodic data received from peer.
 
uint8 dataLen
 Periodic data length.
 
uint8 dataStatus
 Periodic data status.
 
osal_event_hdr_t hdr
 osal event header
 
int8 rssi
 RSSI of the received packet.
 
uint16 syncHandle
 sync handle
 
int8 txPower
 Tx Power information.
 

Detailed Description

LE Periodic Advertising Report event.


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale