SYS/BIOS  7.00
Enumerations | Functions
svcHandler.h File Reference

Go to the source code of this file.

Enumerations

enum  svc_num_t {
  TZ_INIT_CONTEXT_SYSTEM,
  TZ_ALLOC_MODULE_CONTEXT,
  TZ_FREE_MODULE_CONTEXT,
  TZ_LOAD_CONTEXT,
  TZ_STORE_CONTEXT
}
 

Functions

uint32_t initContextSystem ()
 
uint32_t allocModuleContext (uint32_t modId)
 
uint32_t freeModuleContext (uint32_t modId)
 
uint32_t loadContext (uint32_t modId)
 
uint32_t storeContext (uint32_t modId)
 

Enumeration Type Documentation

§ svc_num_t

enum svc_num_t
Enumerator
TZ_INIT_CONTEXT_SYSTEM 
TZ_ALLOC_MODULE_CONTEXT 
TZ_FREE_MODULE_CONTEXT 
TZ_LOAD_CONTEXT 
TZ_STORE_CONTEXT 

Function Documentation

§ initContextSystem()

uint32_t initContextSystem ( )

§ allocModuleContext()

uint32_t allocModuleContext ( uint32_t  modId)

§ freeModuleContext()

uint32_t freeModuleContext ( uint32_t  modId)

§ loadContext()

uint32_t loadContext ( uint32_t  modId)

§ storeContext()

uint32_t storeContext ( uint32_t  modId)
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale