SYS/BIOS
7.00
|
The Load module reports execution times and load information for threads in a system.
SYS/BIOS manages four distinct levels of execution threads: hardware interrupt service routines, software interrupt routines, tasks, and background idle functions. This module reports execution time and load on a per-task basis, and also provides information globally for hardware interrupt service routines, software interrupt routines and idle functions (in the form of the idle task). It can also report an estimate of the global CPU load.
Execution time is reported in units of Timestamp counts, and load is reported in percentages.
By default, load data is gathered for Task threads. Load_hwiEnabled, Load_swiEnabled and Load_taskEnabled can be used to select which type(s) of threads are monitored. Users can also choose to call Load_getTaskLoad, Load_getGlobalSwiLoad, Load_getGlobalHwiLoad and Load_getCPULoad at any time to obtain the statistics at runtime.
The module relies on Load_update to be called to compute load and execution times from the time when Load_update was last called. This is automatically done for every period specified by Load_windowInMs in an Idle function when Load_updateInIdle is set to true. The time between two calls to Load_update is called the benchmark time window.
By passing in a function pointer of type void(*Load_postUpdate)(void) through the Load_postUpdate config parameter, one can specify a Load_postUpdate function that is automatically called by Load_update immediately after the statistics have been computed at the end of a benchmark time window. Setting this function allows the user to optionally post-process the thread statistics once and only once per benchmark window.
Advanced users could optionally omit calling Load_update in the idle loop by setting Load_updateInIdle to false. They can then call Load_update somewhere else (e.g. in a periodic higher priority Task) instead to ensure statistics are computed even when the system is never idle.
The CPU load is computed in three different ways, depending on what threads are monitored, and whether or not Power management is used to idle the CPU when no threads are running.
Task Load Disabled and No Power Management
The first method of calculating CPU load is used when Task load monitoring is disabled, ie, Load_taskEnabled is false, and Power management is not used. The CPU load is computed as the percentage of time in the benchmark window which was NOT spent in the idle loop. More specifically, the load is computed as follows:
global CPU load = 100 * (1 - (min. time for a trip around idle loop * # times in idle loop)/(benchmark time window) )
Any work done in the idle loop is included in the CPU load - in other words, any time spent in the loop beyond the shortest trip around the idle loop is counted as non-idle time.
This method works fairly well if the timestamp frequency is sufficiently high (for example, if it's equal to the CPU frequency). The CPU load accuracy can also be affected by caching and user idle functions.
Task Load Enabled and No Power Management
The second method of calculating CPU load is used when Task load monitoring is enabled (Load_taskEnabled = true) and Power management is not used. In this case the CPU load is calculted as
global CPU load = 100 - (Idle task load)
This prevents any discrepancy between the calculated CPU load had we used the first method, and 100 - the Idle task load. If Swi and Hwi load monitoring are not enabled, however, time spent in a Swi or Hwi will be charged to the task in which it ran. This will affect the accuracy of the CPU (and Task) load, but the trade off is more overhead to do the Hwi and Swi load monitoring.
Power Management Enabled
The Load module is dependent on the timestamp timer, thus the latter must continue to run during idle, in order to accurately measure idle and non-idle time. On platforms where the timestamp timer is halted during sleep (e.g. CC32XX), the Load module can only report correct numbers when power management is disabled. On other platforms where the timer continues to run during sleep, the best way to get CPU load is to make sure that Load_taskEnabled is set to true. Then the CPU load will be calculated as 100 - the idle task load. However, for BIOS in ROM builds, this method will not work, as Task hooks are not allowed. So to use Load for any devices that support BIOS in ROM builds, make sure the ROM build is disabled.
Function | Hwi | Swi | Task | Main | Startup |
---|---|---|---|---|---|
getCPULoad | Y | Y | Y | N | N |
getGlobalHwiLoad | Y | Y | Y | N | N |
getGlobalSwiLoad | Y | Y | Y | N | N |
getTaskLoad | Y | Y | Y | N | N |
reset | Y* | Y* | Y | Y | N |
update | Y* | Y* | Y | N | N |
Definitions:
|
#include <xdc/std.h>
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/sysbios/knl/Queue.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/hal/Hwi.h>
#include <ti/sysbios/runtime/Error.h>
#include "Load_defs.h"
Go to the source code of this file.
Data Structures | |
struct | Load_Stat |
Load statistics info. More... | |
struct | Load_Module_State |
Macros | |
#define | ti_sysbios_utils_Load_long_names |
#define | Load_module ((Load_Module_State *) &(Load_Module_state)) |
Typedefs | |
typedef void(* | Load_FuncPtr) (void) |
Callback function type. More... | |
Functions | |
void | Load_init (void) |
bool | Load_getTaskLoad (Task_Handle task, Load_Stat *stat) |
Return the load and time spent in a specific task. More... | |
void | Load_update () |
Record thread statistics and reset all counters. More... | |
void | Load_reset () |
Reset all internal load counters. More... | |
bool | Load_getGlobalSwiLoad (Load_Stat *stat) |
Return the load and time spent in Swi's. More... | |
bool | Load_getGlobalHwiLoad (Load_Stat *stat) |
Return the load and time spent in hwi's. More... | |
uint32_t | Load_getCPULoad () |
Return an estimate of the global CPU load. More... | |
uint32_t | Load_calculateLoad (Load_Stat *stat) |
Compute total CPU load from a Load_Stat structure. More... | |
uint32_t | Load_setMinIdle (uint32_t newMinIdleTime) |
Set lower bound on idle loop time used to compute CPU load. More... | |
void | Load_addTask (Task_Handle task, Load_HookContext *env) |
Add a task to the list for benchmarking. More... | |
bool | Load_removeTask (Task_Handle taskHandle) |
Remove a task from the list for benchmarking. More... | |
#define ti_sysbios_utils_Load_long_names |
#define Load_module ((Load_Module_State *) &(Load_Module_state)) |
typedef void(* Load_FuncPtr) (void) |
Callback function type.
void Load_init | ( | void | ) |
bool Load_getTaskLoad | ( | Task_Handle | task, |
Load_Stat * | stat | ||
) |
Return the load and time spent in a specific task.
This function returns the load and time spent in a specific task along with the duration over which the measurement was done. Numbers are reported in Timestamp counts.
Task handle must be valid and have been registered with Load.
task | Handle of the Task which time we are interested in. |
stat | Load and time statistics info |
true | if success, false if failure |
void Load_update | ( | ) |
Record thread statistics and reset all counters.
If Load_taskEnabled is set to true, this function can only be called in task context.
void Load_reset | ( | ) |
Reset all internal load counters.
If Load_taskEnabled is set to true, this function can only be called in task context.
bool Load_getGlobalSwiLoad | ( | Load_Stat * | stat | ) |
Return the load and time spent in Swi's.
This function returns the load and time spent in Swi's along with the time duration over which the measurement was done. Numbers are reported in Timestamp counts.
stat | Load and time statistics info |
true | if success, false if failure |
bool Load_getGlobalHwiLoad | ( | Load_Stat * | stat | ) |
Return the load and time spent in hwi's.
This function computes the load and time spent in Hwi's along with the time duration over which the measurement was done. Numbers are reported in Timestamp counts.
stat | Load and time statistics info |
true | if success, false if failure |
uint32_t Load_getCPULoad | ( | ) |
Return an estimate of the global CPU load.
This function returns an estimate of CPU load (% utilization of the CPU), with the idle time determined based on number of trips through the idle loop multiplied by the shortest amount of time through the loop.
This function requires the idle loop to be run during a benchmark time window.
Note: Time spent in kernel while switching to a Hwi/Swi/Task is considered non-idle time.
CPU | load in % |
uint32_t Load_calculateLoad | ( | Load_Stat * | stat | ) |
uint32_t Load_setMinIdle | ( | uint32_t | newMinIdleTime | ) |
Set lower bound on idle loop time used to compute CPU load.
void Load_addTask | ( | Task_Handle | task, |
Load_HookContext * | env | ||
) |
Add a task to the list for benchmarking.
If Load_taskEnabled is set to true, this function can only be called in task context.
task | Handle of the Task to be added to the list. |
env | Handle of context structure to be used by the Task |
bool Load_removeTask | ( | Task_Handle | taskHandle | ) |
Remove a task from the list for benchmarking.
If Load_taskEnabled is set to true, this funciton can only be called in task context.
taskHandle | Handle of the Task to be removed from the list. |