SYS/BIOS  7.00
Data Fields
Hwi_Module_State Struct Reference

#include <ti/sysbios/family/arm/v8m/Hwi.h>

Data Fields

char * taskSP
 
bool excActive
 
void * excContext
 
void * excStack
 
void * isrStack
 
void * isrStackBase
 
unsigned int swiTaskKeys
 
void * isrStackSize
 
void * vectorTableBase
 
void * dispatchTable
 
volatile bool vnvicFlushRequired
 
uint8_t * intAffinity
 
uint32_t * intAffinityMasks
 
Hwi_VectorFuncPtrvectorTable
 
bool initDone
 

Field Documentation

§ taskSP

char* Hwi_Module_State::taskSP

§ excActive

bool Hwi_Module_State::excActive

§ excContext

void* Hwi_Module_State::excContext

§ excStack

void* Hwi_Module_State::excStack

§ isrStack

void* Hwi_Module_State::isrStack

§ isrStackBase

void* Hwi_Module_State::isrStackBase

§ swiTaskKeys

unsigned int Hwi_Module_State::swiTaskKeys

§ isrStackSize

void* Hwi_Module_State::isrStackSize

§ vectorTableBase

void* Hwi_Module_State::vectorTableBase

§ dispatchTable

void* Hwi_Module_State::dispatchTable

§ vnvicFlushRequired

volatile bool Hwi_Module_State::vnvicFlushRequired

§ intAffinity

uint8_t* Hwi_Module_State::intAffinity

§ intAffinityMasks

uint32_t* Hwi_Module_State::intAffinityMasks

§ vectorTable

Hwi_VectorFuncPtr* Hwi_Module_State::vectorTable

§ initDone

bool Hwi_Module_State::initDone

The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale