![]() |
![]() |
TI-15.4 Stack API
5.20.00.15
|
#include <api_mac.h>
Data Fields | |
uint8_t | eBeaconOrder |
uint8_t | offsetTimeSlot |
uint16_t | NBPANEBeaconOrder |
uint8_t * | pIEIDs |
uint8_t | numIEs |
MPM(Multi-PHY layer management) parameters
uint8_t _apimac_mpmParams::eBeaconOrder |
The exponent used to calculate the enhanced beacon interval. A value of 15 indicates no EB in a beacon enabled PAN
uint8_t _apimac_mpmParams::offsetTimeSlot |
Indicates the time diff between the EB and the preceeding periodic Beacon. The valid range for this field is 10 - 15.
uint16_t _apimac_mpmParams::NBPANEBeaconOrder |
Indicates how often the EB to tx in a non-beacon enabled PAN. A value of 16383 indicates no EB in a non-beacon enabled PAN
uint8_t* _apimac_mpmParams::pIEIDs |
pointer to the buffer containing the Information element IDs which needs to be sent in Enhanced Beacon. This field is reserved for future use and should be set to NULL.
uint8_t _apimac_mpmParams::numIEs |
The number of Information Elements in the buffer (size of buffer at pIEIDs. This field is reserved for future use and should be set to 0.