TI-15.4 Stack API
5.20.00.15
|
#include <api_mac.h>
Data Fields | |
ApiMac_status_t | status |
uint8_t | msduHandle |
uint32_t | timestamp |
uint16_t | timestamp2 |
uint8_t | retries |
uint8_t | mpduLinkQuality |
uint8_t | correlation |
int8_t | rssi |
uint32_t | frameCntr |
MCPS data confirm type
ApiMac_status_t _apimac_mcpsdatacnf::status |
Contains the status of the data request operation
uint8_t _apimac_mcpsdatacnf::msduHandle |
Application-defined handle value associated with the data request
uint32_t _apimac_mcpsdatacnf::timestamp |
The time, in backoffs, at which the frame was transmitted
uint16_t _apimac_mcpsdatacnf::timestamp2 |
The time, in internal MAC timer units, at which the frame was transmitted
uint8_t _apimac_mcpsdatacnf::retries |
The number of retries required to transmit the data frame
uint8_t _apimac_mcpsdatacnf::mpduLinkQuality |
The link quality of the received ack frame
uint8_t _apimac_mcpsdatacnf::correlation |
The raw correlation value of the received ack frame
int8_t _apimac_mcpsdatacnf::rssi |
The RF power of the received ack frame in units dBm
uint32_t _apimac_mcpsdatacnf::frameCntr |
Frame counter value used (if any) for the transmitted frame