Radio Software Bundle (rflib) 6.20.00.14 Release Notes
Table of Contents
Introduction
The Radio Software Bundle (RFLib) component for CC13xx and CC26xx consists of:
- The high-level RF driver
- SysConfig meta data for configuring the RF driver and the front-end
- SysConfig meta data for configuring radio PHYs
- Low-level radio access functions used by the RF driver
- RF Core firmware patches for various PHYs
- API documentation
Documentation
The following documentation is included in RFLib.
- RFLib Software Manifest
- API documentation
- Release Notes (this document)
Disclaimer
RF Settings and Patches
RF settings and patches for device family cc13x4_cc26x4, as well as device CC1312PSIP, are in alpha state. They are not fully characterized and have only been tested in a limited manner. Support for certain settings and PHYs may be removed in the future.
Please consider this content for evaluation purposes only.
The cc13x1_cc26x1 CPE multi protocol patch (rf_patch_cpe_multi_protocol) will be deprecated and removed in 1Q23. All generated settings using this patch will be updated to refer to the corresponding protocol patches rf_patch_cpe[bt5, ieee_802_15_4, prop].
RF Sysconfig: Antenna Switch Hardware Changes
The antenna switch, available under “Use Hardware”, is required by P device boards (matching regex /CC....P/). To ensure correct RF performance, the correct value for this option is now selected by default in the UI, but not when adding the RF module in a config script.
Make sure this option is selected for correct RF performance. It must also be placed before any assignments related to the RF module for coex.
See snippet below to add correct hardware:
const RF = scripting.addModule("/ti/drivers/RF");
if (("board" in system.deviceData) && ("RF" in system.deviceData.board.components)) {
RF.$hardware = system.deviceData.board.components.RF;
}What’s New
| ID | Summary |
|---|---|
| RFDRIVER-496 | Removed TI ARM-CGT compiler support |
| RFCORE-874 | CC2652PSIP: Settings Release, PA Table Update - 5/10 dBm: BLE 1M, 2M, Coded and IEEE 802.15.4 (ZigBee) - Characterized |
| RFCORE-888 | CC2651RSIPA: Settings Release, PA Table Update - 5 dBm: BLE 1M, 2M, Coded and IEEE 802.15.4 (ZigBee) - Characterized |
| RFCORE-831 | cc13x4_cc26x4: New Feature: Enable IEEE PTA Coexistence |
Fixed Issues
| ID | Summary |
|---|---|
| None | None |
Known Issues
| ID | Summary |
|---|---|
| None | None |
Upgrade and Compatibility Information
This release breaks compatibility with previous releases of RFLib in the following ways:
- Compiler support: The
TI ARM-CGTcompiler is no longer supported. See section “Upcoming Features TI-RTOS7 and TI CLANG” in the top-level SDK release notes.
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.