#include <rf_ieee_cmd.h>
§ nTxAck
uint8_t rfc_ieeeRxOutput_s::nTxAck |
Total number of transmitted ACK frames.
§ nRxBeacon
uint8_t rfc_ieeeRxOutput_s::nRxBeacon |
Number of received beacon frames.
§ nRxData
uint8_t rfc_ieeeRxOutput_s::nRxData |
Number of received data frames.
§ nRxAck
uint8_t rfc_ieeeRxOutput_s::nRxAck |
Number of received acknowledgement frames.
§ nRxMacCmd
uint8_t rfc_ieeeRxOutput_s::nRxMacCmd |
Number of received MAC command frames.
§ nRxReserved
uint8_t rfc_ieeeRxOutput_s::nRxReserved |
Number of received frames with reserved frame type.
§ nRxNok
uint8_t rfc_ieeeRxOutput_s::nRxNok |
Number of received frames with CRC error.
§ nRxIgnored
uint8_t rfc_ieeeRxOutput_s::nRxIgnored |
Number of frames received that are to be ignored.
§ nRxBufFull
uint8_t rfc_ieeeRxOutput_s::nRxBufFull |
Number of received frames discarded because the Rx buffer was full.
§ lastRssi
int8_t rfc_ieeeRxOutput_s::lastRssi |
RSSI of last received frame.
§ maxRssi
int8_t rfc_ieeeRxOutput_s::maxRssi |
Highest RSSI observed in the operation.
§ __dummy0
uint8_t rfc_ieeeRxOutput_s::__dummy0 |
§ beaconTimeStamp
ratmr_t rfc_ieeeRxOutput_s::beaconTimeStamp |
Time stamp of last received beacon frame.
The documentation for this struct was generated from the following file: