#include <rf_hid_cmd.h>
|
uint8_t | nTx |
| Number of packets or acknowledgements transmitted. More...
|
|
uint8_t | nRxOk |
| Number of packets that have been received with CRC OK. More...
|
|
uint8_t | nRxNok |
| Number of packets that have been received with CRC error. More...
|
|
uint8_t | nRxIgnored |
| Number of packets ignored as retransmissions or empty ACKs. More...
|
|
uint8_t | nRxBufFull |
| Number of packets that have been received and discarded due to lack of buffer space. More...
|
|
uint8_t | nRxAborted |
| Number of packets not received due to device address mismatch, invalid length, or abort command. More...
|
|
uint8_t | __dummy0 |
|
int8_t | lastRssi |
| RSSI of last received packet. More...
|
|
ratmr_t | timeStamp |
| Time stamp of last received packet. More...
|
|
§ nTx
uint8_t rfc_hidRxTxOutput_s::nTx |
Number of packets or acknowledgements transmitted.
§ nRxOk
uint8_t rfc_hidRxTxOutput_s::nRxOk |
Number of packets that have been received with CRC OK.
§ nRxNok
uint8_t rfc_hidRxTxOutput_s::nRxNok |
Number of packets that have been received with CRC error.
§ nRxIgnored
uint8_t rfc_hidRxTxOutput_s::nRxIgnored |
Number of packets ignored as retransmissions or empty ACKs.
§ nRxBufFull
uint8_t rfc_hidRxTxOutput_s::nRxBufFull |
Number of packets that have been received and discarded due to lack of buffer space.
§ nRxAborted
uint8_t rfc_hidRxTxOutput_s::nRxAborted |
Number of packets not received due to device address mismatch, invalid length, or abort command.
§ __dummy0
uint8_t rfc_hidRxTxOutput_s::__dummy0 |
§ lastRssi
int8_t rfc_hidRxTxOutput_s::lastRssi |
RSSI of last received packet.
§ timeStamp
ratmr_t rfc_hidRxTxOutput_s::timeStamp |
Time stamp of last received packet.
The documentation for this struct was generated from the following file: